Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:tools:m2k:accessories:bnc [15 Jun 2021 15:29] – Numbered figures Pop Andreeauniversity:tools:m2k:accessories:bnc [14 Mar 2022 10:17] (current) Pop Andreea
Line 1: Line 1:
-======  ADALM2000 BNC Adapter Board======+======  ADALM2000 BNC Adapter Board ======
  
  
  
-The AD-M2KBNC-EBZ is an ADALM2000 add-on board which allows the user to connect oscilloscope probes and other test leads to the analog inputs of M2K. +The [[adi>AD-M2KBNC-EBZ]] is an [[adi>ADALM2000]] add-on board which allows the user to connect oscilloscope probes and other test leads to the analog inputs of M2K. 
  
  
-{{:university:tools:m2k:accessories:bnc_b.png?400|}} 
  
  
-Figure 1. AD-M2KBNC-EBZ Top view+{{:university:tools:m2k:accessories:ad-m2kbnc-ebz-top-web.png?300|}} 
 +{{:university:tools:m2k:accessories:ad-m2kbnc-ebz-bottom-web.png?300|}} 
 + 
 + 
 + 
 + 
 + 
 + 
 +Figure 1. AD-M2KBNC-EBZ Top view and bottom view
 ===== Features ===== ===== Features =====
   * AC or  DC coupling on all channels   * AC or  DC coupling on all channels
   * Possibility to reconfigure the analog inputs as differential input channels   * Possibility to reconfigure the analog inputs as differential input channels
   * Access to all other ADALM2000 output pins   * Access to all other ADALM2000 output pins
 +  * Oscilloscope probes, BNC to grabber cables and  mini grabber test clips are included in the package
  
 ===== Description ===== ===== Description =====
Line 27: Line 35:
 ===== Package contents ===== ===== Package contents =====
   * AD-M2KBNC-EBZ   * AD-M2KBNC-EBZ
-  * 2 x Oscilloscope Probes +  * 2 x Oscilloscope Probes (PA360 60MHz x1 & x10 Passive Probe) 
-  * 2 x BNC to grabber cables+  * 2 x BNC to grabber cables 
   * 10 x mini grabber test clips   * 10 x mini grabber test clips
  
-{{:university:tools:m2k:accessories:bnc_a.png?300|}} + 
-{{:university:tools:m2k:accessories:bnc_acc.png?500|}}+ 
 +{{ :university:tools:m2k:accessories:ad-m2kbnc-ebz-angle-web.png?600 |}} 
 + 
 +{{:university:tools:m2k:accessories:ad-m2kbnc-ebz_oscilloscope_probes-web.png?250 |}} 
 +{{:university:tools:m2k:accessories:ad-m2kbnc-ebz_bnc_to_grabber_cables-web.png?250 |}} 
 +{{:university:tools:m2k:accessories:ad-m2kbnc-ebz_mini_grabber_test_clips-web.png?250|}}
  
 <WRAP centeralign> Figure 2. AD-M2KBNC-EBZ Isometric view - Package contents </WRAP> <WRAP centeralign> Figure 2. AD-M2KBNC-EBZ Isometric view - Package contents </WRAP>
 +
 +----
  
 ===== Getting started===== ===== Getting started=====
Line 40: Line 55:
 The BNC adapter board is simply plugged into the ADALM2000 and can be used straight away. It does not need any supply or additional circuitry.  The BNC adapter board is simply plugged into the ADALM2000 and can be used straight away. It does not need any supply or additional circuitry. 
  
-{{ :university:tools:m2k:accessories:20210607_103726.jpg?400 |}}+{{ :university:tools:m2k:accessories:20220314_104919.jpg?400 |}}
 <WRAP centeralign> Figure 3. AD-M2KBNC-EBZ connected to ADALM2000 </WRAP> <WRAP centeralign> Figure 3. AD-M2KBNC-EBZ connected to ADALM2000 </WRAP>
 +
 +====AC/DC Coupling ====
 +
 +{{ :university:tools:m2k:accessories:coupling_highlight.png?400 |}}
 +<WRAP centeralign> Figure 4. AD-M2KBNC-EBZ jumpers for AD/DC coupling </WRAP>
 +
 +The input and output channels of this board can be AC or DC coupled using the shunt jumpers. In the following table is presented the jumper configuration:
 +
 +^ Jumper ^    Missing    ^  Jumper 1-2 shorted  ^   Jumper 2-3 shorted  ^
 +|S1- Analog In channel 1  |   inoperable/disconnected |   DC coupled |   AC Coupled|
 +|S2- Analog In channel 2  |   inoperable/disconnected |   DC coupled |   AC Coupled|
 +|P4- Analog Out channel 1 |   inoperable/disconnected |   DC coupled |   AC Coupled|
 +|P5- Analog Out channel 2 |   inoperable/disconnected |   DC coupled |   AC Coupled|
 +
 +
 +
 +
 +====Differential Inputs====
 +
 +The [[adi>AD-M2KBNC-EBZ]] inputs are reconfigurable. By default 1+ and 2+ channels are referenced to the GND of the board and are single ended input channels. There are some solder jumpers on the bottom of the board that allow the user to change the default configuration and use the differential inputs, as ADALM2000 allows this. If the jumpers are soldered as in the table below, the BNC connectors J3 and J4  correspond to channels 1- and 2- of the ADALM2000.
 +
 +
 +^ Solderjumpers shorted pins   ^^^^ BNC connector-M2K pin correspondence ^^^^
 +|JP1|JP2|JP3|JP4|J1|J2|J3|J4|
 +|1 2|1 2|1 2|1 2|1+|2+|W1|W2| 
 +|2 3|2 3|2 3|2 3|1+|2+|1-|2-| 
 +
 +{{:university:tools:m2k:accessories:input_path_single_ended.png?400|}}
 +{{:university:tools:m2k:accessories:input_path_differential.png?400|}}
 +
 +<WRAP centeralign> Figure 5. AD-M2KBNC-EBZ bottom solderjumpers(left-single ended inputs, right-differential inputs)</WRAP>
 +
 +===== Schematics and CAD Files =====
 +<WRAP round download>
 +
 +  * {{ :university:tools:m2k:accessories:02-064107-01-b.pdf  |Rev B Schematics}}
 +  * {{ :university:tools:m2k:accessories:09-064107-01b.zip |Rev B Gerbers}}
 +  * {{ :university:tools:m2k:accessories:20-064107-01b.zip |Rev B Cadence Project}}
 +</WRAP>
 +
university/tools/m2k/accessories/bnc.1623763794.txt.gz · Last modified: 15 Jun 2021 15:29 by Pop Andreea