Wiki

This version (14 Mar 2022 10:17) was approved by Pop Andreea.The Previously approved version (14 Mar 2022 10:16) is available.Diff

ADALM2000 BNC Adapter Board

The AD-M2KBNC-EBZ is an ADALM2000 add-on board which allows the user to connect oscilloscope probes and other test leads to the analog inputs of M2K.

Figure 1. AD-M2KBNC-EBZ Top view and bottom view

Features

  • AC or DC coupling on all channels
  • Possibility to reconfigure the analog inputs as differential input channels
  • Access to all other ADALM2000 output pins
  • Oscilloscope probes, BNC to grabber cables and mini grabber test clips are included in the package

Description

The AD-M2KBNC-EBZ has 2 single ended input channels and 2 single ended output channels. All these channels are terminated in a right-angle BNC connector which provides quick connection and a locking mechanism. The single ended input channels can be reconfigured as differential input channels by modifying a solder jumper on the bottom of the board. In this way, all 4 BNC connectors will be used for the analog input section and the output of the M2K is still available on the 30 pin header of the board.

Applications

  • Electronic test and measurement equipment
  • General-purpose signal processing applications
  • Automated test equipment
  • Educational applications

Package contents

  • AD-M2KBNC-EBZ
  • 2 x Oscilloscope Probes (PA360 60MHz x1 & x10 Passive Probe)
  • 2 x BNC to grabber cables
  • 10 x mini grabber test clips

Figure 2. AD-M2KBNC-EBZ Isometric view - Package contents


Getting started

The BNC adapter board is simply plugged into the ADALM2000 and can be used straight away. It does not need any supply or additional circuitry.

Figure 3. AD-M2KBNC-EBZ connected to ADALM2000

AC/DC Coupling

Figure 4. AD-M2KBNC-EBZ jumpers for AD/DC coupling

The input and output channels of this board can be AC or DC coupled using the shunt jumpers. In the following table is presented the jumper configuration:

Jumper Missing Jumper 1-2 shorted Jumper 2-3 shorted
S1- Analog In channel 1 inoperable/disconnected DC coupled AC Coupled
S2- Analog In channel 2 inoperable/disconnected DC coupled AC Coupled
P4- Analog Out channel 1 inoperable/disconnected DC coupled AC Coupled
P5- Analog Out channel 2 inoperable/disconnected DC coupled AC Coupled

Differential Inputs

The AD-M2KBNC-EBZ inputs are reconfigurable. By default 1+ and 2+ channels are referenced to the GND of the board and are single ended input channels. There are some solder jumpers on the bottom of the board that allow the user to change the default configuration and use the differential inputs, as ADALM2000 allows this. If the jumpers are soldered as in the table below, the BNC connectors J3 and J4 correspond to channels 1- and 2- of the ADALM2000.

Solderjumpers shorted pins BNC connector-M2K pin correspondence
JP1JP2JP3JP4J1J2J3J4
1 21 21 21 21+2+W1W2
2 32 32 32 31+2+1-2-

Figure 5. AD-M2KBNC-EBZ bottom solderjumpers(left-single ended inputs, right-differential inputs)

Schematics and CAD Files

university/tools/m2k/accessories/bnc.txt · Last modified: 14 Mar 2022 10:17 by Pop Andreea