This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:accessories:bnc [15 Jun 2021 15:29] – Numbered figures Pop Andreea | university:tools:m2k:accessories:bnc [14 Mar 2022 10:17] (current) – Pop Andreea | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
- | The AD-M2KBNC-EBZ is an ADALM2000 add-on board which allows the user to connect oscilloscope probes and other test leads to the analog inputs of M2K. | + | The [[adi>AD-M2KBNC-EBZ]] is an [[adi>ADALM2000]] add-on board which allows the user to connect oscilloscope probes and other test leads to the analog inputs of M2K. |
- | {{: | ||
- | Figure 1. AD-M2KBNC-EBZ Top view | + | {{: |
+ | {{: | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | Figure 1. AD-M2KBNC-EBZ Top view and bottom | ||
===== Features ===== | ===== Features ===== | ||
* AC or DC coupling on all channels | * AC or DC coupling on all channels | ||
* Possibility to reconfigure the analog inputs as differential input channels | * Possibility to reconfigure the analog inputs as differential input channels | ||
* Access to all other ADALM2000 output pins | * Access to all other ADALM2000 output pins | ||
+ | * Oscilloscope probes, BNC to grabber cables and mini grabber test clips are included in the package | ||
===== Description ===== | ===== Description ===== | ||
Line 27: | Line 35: | ||
===== Package contents ===== | ===== Package contents ===== | ||
* AD-M2KBNC-EBZ | * AD-M2KBNC-EBZ | ||
- | * 2 x Oscilloscope Probes | + | * 2 x Oscilloscope Probes |
- | * 2 x BNC to grabber cables | + | * 2 x BNC to grabber cables |
* 10 x mini grabber test clips | * 10 x mini grabber test clips | ||
- | {{: | + | |
- | {{: | + | |
+ | {{ : | ||
+ | |||
+ | {{: | ||
+ | {{: | ||
+ | {{: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | ---- | ||
===== Getting started===== | ===== Getting started===== | ||
Line 40: | Line 55: | ||
The BNC adapter board is simply plugged into the ADALM2000 and can be used straight away. It does not need any supply or additional circuitry. | The BNC adapter board is simply plugged into the ADALM2000 and can be used straight away. It does not need any supply or additional circuitry. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | ====AC/DC Coupling ==== | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | The input and output channels of this board can be AC or DC coupled using the shunt jumpers. In the following table is presented the jumper configuration: | ||
+ | |||
+ | ^ Jumper ^ Missing | ||
+ | |S1- Analog In channel 1 | | ||
+ | |S2- Analog In channel 2 | | ||
+ | |P4- Analog Out channel 1 | | ||
+ | |P5- Analog Out channel 2 | | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ====Differential Inputs==== | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | |||
+ | ^ Solderjumpers shorted pins ^^^^ BNC connector-M2K pin correspondence ^^^^ | ||
+ | |JP1|JP2|JP3|JP4|J1|J2|J3|J4| | ||
+ | |1 2|1 2|1 2|1 2|1+|2+|W1|W2| | ||
+ | |2 3|2 3|2 3|2 3|1+|2+|1-|2-| | ||
+ | |||
+ | {{: | ||
+ | {{: | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ===== Schematics and CAD Files ===== | ||
+ | <WRAP round download> | ||
+ | |||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | </ | ||
+ |