You don't have to be a software engineer in order to leverage device drivers and example code as you are evaluating and prototyping with Analog Devices' data converters and converter-like products. Selection of an ADC, DAC, or sensor often starts by finding something that meets performance requirements (obviously). This may be followed with some experimentation with the device's evaluation board and accompanying software, but at some point you need to “take the next step”. This “next step” could be any one of a wide array of things - wiring the eval board to a prototype of a larger system, deeper characterization using your own benchtop test equipment, or any one of a plethora of random requirements. This tutorial will arm you with a number of tools to this end.
Analog Devices provides an assortment of reference designs for converters of various channel counts, bandwidths, and other functionality, whose drivers fit into the Industrial Input Output (IIO) framework. This framework facilitates robust data transfer to or from the converter into “userspace”, where the user program could be a MATLAB script for device characterization, a Python script that talks to benchtop signal generators and spectrum analyzers via GPIB in addition to the ADI part under test, or a C program embedded in the end product. Most of these involve fairly costly reference design hardware installed on even more costly FPGA platform boards, which, to extract maximum performance, require test equipment exceeding the cost of a luxury car. So the question arises - what is the simplest, lowest cost system that captures the important aspects of these larger systems? $50 total for a Raspberry Pi, SD card, and ADXL345 board sounds like a pretty reasonable deal.
Figure 1. Ultra-simple IIO-based system
A Note on Security: The Raspberry Pi is a fantastic tool, but it can represent a network security gap if used improperly. Our Raspberry Pi will start out configured in a fairly open state - a simple root password, SSH login enabled. This isn't an issue if the Raspberry Pi does not have internet access or is behind a firewall, but if you are going to connect to your network, it's a good idea to change the password to something secure. Refer to this article on Raspberry Pi Security: Securing your Raspberry Pi
A Note on the Tutorial: This tutorial is hands-on, and attempts to be clear and consistent. But there are often several “right” ways of doing a step - choice of editor to modify files on an SD card, using a Windows, Mac, or Linux machine, etc. When in doubt: Just try stuff. Worst case, you'll need to re-burn your SD card to get back to the starting point.
«Overview of Pluto, FMCOMMS boards, LiDAR platform, and comparison to comparison to Raspberry Pi + ADXL345…»
Before we dig too deep into software stuff, let's prepare the hardware. With Figure 1 as a visual aid, make the connections shown in Figure 2. The accelerometer board is a Digilent model Pmod:ACL, available directly from Digilent: ADXL345 Pmod and from various distributors. It is essentially a breakout board for the ADXL345. There are lots of ways to connect boards together, custom adapters, Raspberry Pi prototyping hats, etc. but 5 inch jumpers from Schmartboard: Schmartboard Jumpers are very convenient.
In theory, any Raspberry Pi should work, although it is probably best to use a modern model with a 40-pin expansion header. (The model shown in Figure 1 is a model 3B, version 1.2.)
Note that there are TWO SPI ports - SPI0 and SPI1. We will be using SPI0 (Pins 8, 19, 21, 23)
Figure 2. RPi-Pmod connections
In order to boot the Raspberry Pi, you will need to obtain an SD card “image”, and write (or “burn”) it to a card. We'll talk about where to get the correct image shortly. This is a fairly common step in bringing up embedded computers - Raspberry Pi, BeagleBone, Zedboard, Arrow SoCkit, or any machine that boots from an SD card. Rather than reinventing the wheel, refer to this often cited guide:
which includes instructions for Windows, Mac, and Linux. Most Windows users will head straight for Win32DiskImager (which works on machines that encrypt data being written to external drives since it's writing “raw” data. HOWEVER - beware encryption software when editing configuration files! More on that later…)
Figure 3. Win32DiskImager screenshot
A new SD card is usually preformatted as a single EXFAT partition, usable by all operating system. But after burning an image to the card, it will show up as several partitions, not all of which are visible to all operating systems. So if you burn a card in Windows, and a popup appears saying “This drive needs to be formatted, would you like to format now?”, the answer is NO! Figure 4 shows the SD card partitions before and after burning the image. Attempting to read the partition map in Windows (under Administrative Tools, Disk Management) will show the ext4 partition as “unknown”
Figure 4. SD card partitions before and after “burning”
Helpful Hint: It may happen that an SD card becomes corrupted somehow. This can sometimes be fixed in Windows by opening storage manager in Administrative tools, then removing all partitions, and reformatting as EXFAT (a similar procedure can be followed using fdisk in Linux.) But computers are smart - sometimes too smart - and there are cases where these tools fail to repartition a drive. However - digital cameras are not as smart, and using a digital camera's (such as a Nikon D90) SD card formatting feature will often resurrect a “bricked” card.
Leveraged Learning: Reference designs for popular data acquisition and transciever boards (FMCOMMSx, FMCDAQx, etc.) use Xilinx and Intel platform boards, which boot from an SD card. The procedure is nearly identical to that of burning an SD card for a Raspberry Pi. (See ADI Zynq Image)
What is “ADI Kuiper Linux”? Here's a little glossary:
More information on Raspbian can be found at Raspbian Homepage. Raspbian includes lots of fun stuff - Minecraft, an office suite, web browser, sound processing labs, other games, etc. We won't cover any of that, but do explore on your own!
(More information on the Kuiper Belt can be found at Kuiper_belt)
The SD card image is available here:
Kuiper Linux
Download the compressed xz file, and extract the .img file. (tar.gz files can be extrtracted using 7zip in Windows.) Follow the procedure for burning SD cards above, using an 8G (or larger), high-quality, Class 10 or faster SD card.
At this point, you should be able to:
Note: It is possible to use the Raspberry Pi without a local keyboard, mouse, monitor - see the “Going Headless” section below.
If all goes well, you should see a desktop. Open a terminal and run IIO Oscilloscope:
analog@analog:~$ sudo osc
(Enter the root password, “analog” by default unless you followed the advice above to change it.) You should then see IIO oscilloscope running as shown in Figure 5! Also note that IIO Oscilloscope will run without root privileges, but all devices will be read-only. For example, you won't be able to change the ADXL345's sampling frequency.
Figure 5. Raspberry Pi w/ Raspbian ADI desktop
But… if you look at the IIO oscilloscope panels, where's the ADXL345? Well, the Linux kernel does a bunch of stuff during boot, controlled by various configuration files (remember autoexec.bat and config.sys on old DOS systems?) One of them, /boot/config.txt, is how you tell Linux about what hardware is connected, and the default is NOT the ADXL345… so let's fix that.
When we first powered up the Raspberry Pi, IIO Oscilloscope ran automatically, but didn't find anything. While we do have our ADXL345 physically connected to the board, Linux doesn't know about it yet. How do we tell the Linux kernel what we've connected to the expansion header? The answer is the “Device Tree Overlay”.
While you won't have to do anything more than editing a couple of files in this tutorial, it helps to understand a bit about what is going on under the surface. A “Device Tree” contains information about a system's hardware - what peripherals exist (like displays, memory, USB, Ethernet controllers, GPIO pins, etc.) A “Device Tree Overlay” contains information about additional connected hardware, like our ADXL345. Figure 6 shows a screenshot of the ADXL345's overlay source. It shows that the ADXL345 is connected to the SPI port, using the first CS signal (CS0), the maximum SPI clock frequency is 1MHz, and the interrupt signal is connected to Pin 19 (as shown in the connection diagram above.)
Figure 6. Partial ADXL345 overlay source (dts)
The device tree source is then compiled into a “flattened” device tree that the Linux kernel reads directly. While this process is fairly straightforward, it's beyond the scope of this tutorial. Furthermore, the device tree overlay for this tutorial is already included on the SD card, along with several other overlays for other hardware configurations. (Note that the device tree overlay is specific to a particular device AND how it is connected to the Raspberry Pi. Any changes to the connections - SPI CS line, interrrupt line, etc. will require a corresponding modificaiton to the overlay.) So keeping with the spirit of doing while we're learning, let's configure the overlay for this experiment. The device tree overlay is specified in the config.txt file, which lives in the BOOT partition on the SD card. There are several ways to edit this file - Since the BOOT partition is a FAT filesystem, you can use any text editor on any operating system; Notepad on Windows, Kedit on Linux, etc. Or… if your Raspberry Pi is booted up, you can edit directly on the Pi! Just open a command prompt, and type:
analog@analog:~$ sudo mousepad /boot/config.txt
which will bring up the file in the Mousepad editor. Scroll down until you find the line that begins with “dtoverlay”, and, whatever it happens to be, change it to:
dtoverlay=rpi-adxl345
Figure 7. Editing config.txt directly on Raspberry Pi.
Or if you want to make it easy to revert back, comment out the original line with a pound sign / hashtag:
#dtoverlay=rpi-something-other-than-adxl345 dtoverlay=rpi-adxl345
One last thing worth noting - the default video resolution is 1920×1080. If this causes problems with your monitor, hanging hdmi_group, mode to 2, 58:
hdmi_group=2 hdmi_mode=58
will set the screen resolution to 1680×1050. Information on other video modes is available here:
However you edit the file, save, close, cross your fingers, and… reboot!
If all went well, Linux should have booted, found the ADXL345, and loaded its driver. Run IIO Oscilloscope from the terminal (sudo osc) again. locate the DMM screen, check the ADXL345, select all channels, and click the triangular “play” button. You should see acceleration values displayed as shown in Figure 8.
Figure 8. IIO Oscilloscope showing ADXL345 channels.
IIO Oscilloscope is a great tool for establishing signs of life, but really isn't intended for much more, so let's start digging deeper into how to communicate with the ADXL345 programmatically. Close out of IIO Oscilloscope, open a terminal and enter:
analog@analog:~$ iio_info
You should see the screen filled with information about the ADXL345 - sample rates, “raw” values, scale values, etc. This means that you're ready to start writing programs to do useful stuff with the ADXL345… on the Raspberry Pi itself. But before we go there, let's introduce one more extraordinarily powerful feature of the IIO framework - the ability to communicate remotely over a network connection. This ability is made up of two components: an IIOD server running on the Raspberry Pi, and LibIIO running on the remote machine. LibIIO is cross-platform, so client applications can be written on Windows / Mac / Linux.
Let's take a peek at the IIOD server. In the Raspberry Pi terminal, enter:
analog@analog:~$ ps aux | grep iiod
Which means “list all processes from all users, but only display ones that include the text “iiod””. You should see a process running as shown in Figure 9 below. (Note that this is the login screen for an ADALM2000 - it's all the same.)
And the red line relates this process back to the handy little diagram from What is Libiio? (We will be recycling that diagram - a lot.)
Figure 9. IIOD process
The other piece is libiio on the remote host. LibIIO can be obtained from:
Download and install the appropriate latest version for your remote host (For example, libiio-0.18.g4e22517-Windows-setup.exe for Windows) Once this is done, open a command prompt, and enter
iio_info -u ip:192.168.1.232
(Where the IP address may be different, depending on how you've connected)
Figure 10. iio_info run locally and remotely.
NOW you've got all the pieces for some fun hacking - you can write software that runs directly on the Raspberry Pi and talks to the ADXL345 (which… is conceptually similar to writing software that runs on a Xilinx SoC board and grabs data from an attached high-speed ADC) AND, you can write software on a remote host - useful if you want a larger application that is more appropriate to run on the host, or if you want to grab large amounts of data for analysis.
LibIIO is written natively in C, but there are bindings for MATLAB, C#, and Python. Let's use Python…
Any language that can call a shared library can communicate with libiio. But Python is attractive for getting started for several reasons:
It's FREE It's tremendously popular It's got tons of number crunching libraries It's got tons of libraries for communicating with hardware (It's also really really fun!) And - it's easy to learn. If you've never touched Python before, there are lots of free resources, including this 4-hour course on YouTube from freeCodeCamp.org:
And this very nice interactive tutorial: Learn Python in which code snippets run in the browser (no need to intall Python.)
If you prefer paper, Python for Kids by Jason R. Briggs is a well written books for kids of all ages. (And Learn to Program with Minecraft: Transform Your World with the Power of Python by Craig Richardson is a pretty nice introduction to the idea of communicating over a network connection; the Minecraft world is a process that communicates over network ports.)
There are several choices of Python installations, and which one to use is largely a matter of preference. Anaconda, PyCharm, and Jupyter Notebook will all work just fine.
On Python Versions - We're using Python 3 (3.7 to be specific.) So if you're installing on your remote host, make sure to get a recent version of Python 3. At the moment, Raspbian ADI edition defaults to Python 2.7. This can be changed by entering the following commands:
analog@analog:~$ sudo update-alternatives --install /usr/bin/python python /usr/bin/python2.7 1 analog@analog:~$ sudo update-alternatives --install /usr/bin/python python /usr/bin/python3.7 2
(This only needs to be done once.)
PyADI-IIO (pronounced “Py-odi”1) is like peyote, but with a Py) is a python abstraction module for ADI hardware with IIO drivers to make them easier to use. pyadi-iio can be installed through pip, but if you're reading this, you'll probably want to be hacking around a bit, so go to PyADI-IIO Github Repo and follow the “installing from source” instructions. And note that this can be done on your remote Windows / Mac / Linux host AND… on the Raspberry Pi itself! Git is already installed on Raspbian ADI edition, but may need to be installed on a Windows host. (You can also download the repository as a zip, but cloning will make it easier to update.) And if you're doing this on the Raspberry Pi - remember to set your Python version! (See above.) Make sure you also install the python bindings for libiio, as shown below.
analog@analog:~ $ pip install pylibiio
Now, let's move on to installing pyadi-iio.
analog@analog:~ $ git clone https://github.com/analogdevicesinc/pyadi-iio.git analog@analog:~ $ cd pyadi-iio analog@analog:~/pyadi-iio $ sudo python setup.py install
Note: This requires that your Raspberry Pi be able to access the internet. If you've followed the “headless” instructions below, this will likely not be the case. However - if you have access to a wireless network and your Raspberry Pi has an Ethernet adapter, you can connect in this way. Just click the WiFi icon and log on as you would on any other machine, supplying a password if necessary
Figure 11. WiFi logon
Now it's (almost) trivial to grab data from the ADXL345 used in this tutorial, as well as more complicated hardware. With pyadi-iio installed, you should be able to run the ADXL345 example:
analog@analog:~/pyadi-iio $ cd examples analog@analog:~/pyadi-iio/examples $ python adxl345_example.py
The example program takes a few acceleration readings, shows how to set the sample rate, and shows how to convert values to SI units.
If you're running the example on the remote host, note that the IP address is hardcoded to 192.168.1.232, the address noted for the “headless” configuration below. If your Raspberry Pi's address is different (supplied by DHCP, for example), change it accordingly. The example will also run locally, with the same IP address! But as soon as the IP address changes, the example won't work any more. Since we're running locally, you can set the IP address to the local loopback address:
myacc = adi.adxl345(uri="ip:127.0.0.1")
But since we're running locally, why bother talking through IIOD? Setting the context to local takes care of that:
myacc = adi.adxl345(uri="local:")
But there's one subtlety… run Python as root ( sudo python adxl345_example.py ). The reason is that IIOD runs with root privileges and can read / write to devices. The example script will be able to read just fine, but writing even something as mundane as the sample rate requires root privileges.
«Note - we should look for a more elegant solution, perhaps adding user pi to the wheel group…»
The example script should run just fine on the Raspberry Pi itself, and on the remote host. Try writing a program to read out a hundred samples from each channel (X,Y,Z) and store to a file, or if you're really adventurous, display the 3-axis acceleration as an arrow in a graphical screen.
Putty and TeraTerm are popular (and free) SSH clients that let you log into a console on your Raspberry Pi (or other remote client). They are available at PuTTY Homepage and TeraTerm Homepage , respectively. Try both, which one is better is largely a matter of preference.
On Mac and Linux machines, you can simply log in via ssh from the command line.
WinSCP is a handy tool that lets you copy files between a Windows machine and your Raspberry Pi, for example, let's say you collect some data on your Pi using a Python script, and want to get it over to your Windows machine. It is available from WinSCP Homepage.
As with SSH, Mac and Linux machines include SCP already.
VNC is a remote desktop application, and Raspbian ADI runs a VNC server by default. There are several clients available; RealVNC works well and is available at RealVNC Viewer A screenshot of VNC logged into the Raspberry Pi is shown in Figure 12.
Figure 12. VNC desktop
(Ignore if you're using a monitor / keyboard / mouse) If it happens that you don't have a spare monitor / keyboard / mouse, or it's just inconvenient, you can operate the Raspberry Pi with only a network connection. There are several ways to do this - if your network has a DHCP server, and you can find the IP address that it assigned to the Raspberry Pi, you're all set. But a very robust way is to set the Raspberry Pi's address manually, and do the same to one network adapter on the host. To set the Raspberry Pi's address, open the boot partition on a host machine (once again… BEWARE ENCRYPTION!), and note that this host machine could be the Raspberry Pi itself, with a montior / keyboard / mouse attached. Open the file “cmdline.txt” and add the following to the end:
ip=192.168.1.232::192.168.1.1:255.255.255.0:rpi:eth0:off
where, the 192.168.1.232 is somewhat arbitrary - just make sure that the first 3 octets (192.168.1) are DIFFERENT from those of any other network adapters on your host machine. The next step is to configure your host's network adapter. Open your computer's “Network Connections” control panel note that your host could have lots of adapters. Sometimes it's obvious - if you're using a cable connection, it's obviously NOT your wifi adapter. If you're using a USB-Ethernet adapter (a super convenient option sometimes), plugging and unplugging the adapter, and seeing which disappears. Open the adapter's configuration (right-click, “Properties”) and configure the IPV4 properties as shown in Figure 13 below. Make sure the last octet in the IP address is DIFFERENT from that set on the Raspberry Pi.
Figure 13. Setting Up Static IP on Windows Host
Finally… open a command prompt, and ping your Raspberry Pi as shown in Figure 14:
Figure 14. Pinging the Headless Pi
If you get a reply, you're all set! You can now log into the Raspberry Pi using PuTTY, VNC, and talk to attached IIO devices via IIO oscilloscope or libiio on the remote host.
«ToDo: see if Avahi is enabled by default (raspberrypi.local? analog.local?) »
Leveraged Learning: This process (and any frustrations accompanied on the way) is the same for using any network connected embedded computer, test equipment, etc.
You're now armed to start building interesting application circuits with the ADXL345, starting with a solid software foundation. Applications can either be connected to a host computer, or can run remotely on the Raspberry Pi itself. Hopefully you're left with one of two feelings: