This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:engineering_discovery:lab_11 [05 Oct 2016 23:09] – [Procedure] Jonathan Pearson | university:courses:engineering_discovery:lab_11 [19 Oct 2016 17:28] – [Procedure] Jonathan Pearson | ||
---|---|---|---|
Line 33: | Line 33: | ||
- Run PixelPulse and plug in the M1K using the supplied USB cable | - Run PixelPulse and plug in the M1K using the supplied USB cable | ||
- Update M1K firmware, if necessary | - Update M1K firmware, if necessary | ||
+ | - Disable “Repeated Sweep” mode; waveforms can be paused for analysis | ||
- Set up the M1K to source voltage/ | - Set up the M1K to source voltage/ | ||
- Set up Channel A source waveform for a 100 Hz “Sine” output that swings between 2.0 V and of 4.0 V | - Set up Channel A source waveform for a 100 Hz “Sine” output that swings between 2.0 V and of 4.0 V |