Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
university:courses:electronics:m2k-uart-debug [21 May 2019 19:26] – Add reference to CLI demo, note about switch position. Mark Thoren | university:courses:electronics:m2k-uart-debug [03 Jan 2021 22:21] (current) – fix links Robin Getz |
---|
| |
**EVAL-ADICUP3029 UART switch configuration:** | **EVAL-ADICUP3029 UART switch configuration:** |
Set S2 to the CENTER position. | |
| * Set S2 to the CENTER position. |
(S2 selects which device to connect the ADuCM3029's UART to - USB-UART interface, Arduino headers, or WiFi module connector.) | (S2 selects which device to connect the ADuCM3029's UART to - USB-UART interface, Arduino headers, or WiFi module connector.) |
| |
| |
====Further Reading:==== | ====Further Reading:==== |
* [[https://www.analog.com/media/en/technical-documentation/application-notes/an-1435.pdf|Implementing UART Using the ADuCM3027/ADuCM3029 Serial Ports ]] | * [[adi>media/en/technical-documentation/application-notes/an-1435.pdf|Implementing UART Using the ADuCM3027/ADuCM3029 Serial Ports ]] |
* [[https://www.analog.com/media/en/technical-documentation/application-notes/EE-391.pdf|Implementing UART Using ADuCM302x Serial Ports]] | * [[adi>media/en/technical-documentation/application-notes/EE-391.pdf|Implementing UART Using ADuCM302x Serial Ports]] |
* [[resources:eval:user-guides:eval-adpaq3029:resources:app_uart|EVAL-ADPAQ3029 - UART(Arduino) demo]] | * [[resources:eval:user-guides:eval-adpaq3029:resources:app_uart|EVAL-ADPAQ3029 - UART(Arduino) demo]] |
* [[resources:eval:user-guides:eval-adicup3029|EVAL-ADICUP3029 User Guide]] | * [[resources:eval:user-guides:eval-adicup3029|EVAL-ADICUP3029 User Guide]] |