This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:m2k-uart-debug [25 Mar 2019 15:15] – Antoniu Miclaus | university:courses:electronics:m2k-uart-debug [03 Jan 2021 22:21] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 5: | Line 5: | ||
The objective of this tutorial is to use the Pattern Generator and Logic Analyzer instruments provided by the [[adi> | The objective of this tutorial is to use the Pattern Generator and Logic Analyzer instruments provided by the [[adi> | ||
- | As an example we will use as second device the [[adi> | + | The [[adi> |
===== Background ==== | ===== Background ==== | ||
- | Universal Asynchronous Receiver/ | + | A Universal Asynchronous Receiver/ |
- | The UART transmit | + | The UART transmitter |
<WRAP centeralign> | <WRAP centeralign> | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | UART transmits data asynchronously, | + | A UART transmits data asynchronously, |
{{: | {{: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | When the UART receive | + | When the UART receiver |
- | UART transmitted | + | UART data is organized into bytes. Each byte contains 1 start bit, 5 to 9 data bits (depending on the UART), an optional parity bit, and 1 or 2 stop bits. |
<WRAP centeralign> | <WRAP centeralign> | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
- | The UART data transmission line is normally held at a high voltage level when no transmission is occurring. To start the transfer of data, the the transmission line is pulled from high to low. When the receiving UART detects the high to low voltage transition, it begins reading the bits in the data frame at the frequency of the baud rate. | + | The UART data transmission line is normally held at a high voltage level when no transmission is occurring. To start the transfer of data, the the transmission line is pulled from high to low. When the receiving UART detects the high to low voltage transition, it interprets this event as as start bit and begins reading |
- | Parity describes the evenness or oddness of a number. The parity bit is a way for the receiving UART to tell if any data has changed during transmission. Bits can be changed by mismatched baud rates, long distance data transfers, etc. After the receiving UART reads the data frame, it counts the number of bits with a value of 1 and checks if the total is an even or odd number. If the parity bit is a 0 (even parity), the 1 bits in the data frame should total to an even number. If the parity bit is a 1 (odd parity), the 1 bits in the data frame should total to an odd number. When the parity bit matches the data, the UART knows that the transmission was free of errors. | + | A parity bit may be included after the data bits. Parity describes |
- | To signal the end of the data packet, the sending UART drives the data transmission line from a low voltage to a high voltage for at least two bit durations. | + | Even parity: for a given set of bits, the occurrences of bits whose value is 1 is counted. If that count is odd, the parity bit value is set to 1. If the count of 1s in a given set of bits is already even, the parity bit value is 0. |
+ | |||
+ | Odd parity: for a given set of bits, if the count of bits with a value of 1 is even, the parity bit value is set to 1 . If the count of bits with a value of 1 is odd, the count is already odd so the parity bit value is 0. | ||
+ | |||
+ | The parity bit is simple error detection scheme, and will detect all single-bit errors. Bits can be changed during transmission by mismatched baud rates, noise picked up on long distance data transfers, etc. Like baud rate, both transmitter and receiver must be set to the same parity configuration. | ||
+ | |||
+ | To signal the end of the data byte, the sending UART drives the data transmission line from a low voltage to a high voltage for at least two bit periods. | ||
===== Hardware Configuration ==== | ===== Hardware Configuration ==== | ||
- | Figure 4. shows the hardware connection between M2K board and EVAL-ADICUP360 + EVAL-CN0411-ARDZ shield. | + | Figure 4. shows the hardware connection between M2K board and EVAL-ADICUP3029. |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 42: | Line 48: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | The UART pins for the EVAL-ADICUP3029 are available for communication at port **P7**. | ||
+ | |||
+ | **EVAL-ADICUP3029 UART pin configuration: | ||
+ | PORT P7: | ||
+ | * Pin7 - UART TX | ||
+ | * Pin8 - UART RX | ||
+ | |||
+ | PORT P4: | ||
+ | * Pin7 - GND | ||
+ | |||
+ | **M2K UART pin configuration: | ||
+ | * DIO0 - TX | ||
+ | * DIO1 - RX | ||
+ | * GND - DGND | ||
+ | |||
+ | Connect M2K pins to EVAL-ADICUP3029 as follows: | ||
+ | * Pin7 - DIO1 | ||
+ | * Pin8 - DIO0 | ||
+ | |||
+ | **EVAL-ADICUP3029 UART switch configuration: | ||
+ | |||
+ | * Set S2 to the CENTER position. | ||
+ | |||
+ | (S2 selects which device to connect the ADuCM3029' | ||
+ | |||
+ | ===== Software Configuration ==== | ||
+ | |||
+ | There are several options for which software to use for this demonstration; | ||
+ | |||
+ | [[https:// | ||
+ | |||
+ | |||
+ | |||
+ | ===== Scopy Pattern Generator Configuration ==== | ||
+ | |||
+ | First, set up the Pattern Generator to transmit test data to EVAL-ADICUP3029. | ||
+ | |||
+ | The EVAL-ADICUP3029 software application has the UART configured as follows: | ||
+ | * Baud rate: 115200 | ||
+ | * Stop bits: 1 | ||
+ | * Parity: none | ||
+ | |||
+ | For transmission, | ||
+ | |||
+ | On the left side of the user interface, a settings menu is available. Configure the UART settings to match the software application that we want to debug. | ||
+ | |||
+ | An example for the Pattern Generator setup is presented in Figure 5. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | **Pattern Generator settings:** | ||
+ | * Pattern: UART | ||
+ | * Baud: 115200 | ||
+ | * Stop bits: 1 | ||
+ | * Parity: None | ||
+ | * Data to send: ' | ||
+ | |||
+ | ===== Scopy Logic Analyzer Configuration ==== | ||
+ | |||
+ | Several UART configuration parameters need to be determined in order to properly configure Scopy. For the EVAL-ADICUP3029 project, they are as follows: | ||
+ | * Baud rate: 115200 | ||
+ | * Data bits: 8 | ||
+ | * Parity: none (Check polarity: no) | ||
+ | * Stop bits: 1 | ||
+ | * Bit order: LSB first | ||
+ | * Data format: ASCII | ||
+ | |||
+ | An overview of the user interface is shown in Figure 6. | ||
+ | |||
+ | {{: | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | Open the Logic Analyzer instrument, select DIO0-DIO1 lines and press the "Group with selected" | ||
+ | |||
+ | Select the channel group formed and apply the UART decoder. While the group is selected, open settings menu by pressing the {{: | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | The Logic Analyzer must be set up to “catch” the UART byte transfer on the Logic Analyzer plot. Since the UART transfer starts with a start bit, (transmit line is pulled from high to low), we can use this event to trigger the capture. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | |||
+ | ===== UART Example ===== | ||
+ | |||
+ | This example verifies the receive/ | ||
+ | The data will be transmitted from the Pattern Generator, and visualized on Logic Analyzer, by connecting ADALM2000 to the UART pins of the EVAL-ADICUP3029 board (see Hardware Configuration step). | ||
+ | |||
+ | Set the Time Base of the Logic Analyzer instrument to 30us and the Trigger Position at 90us and run a Single sweep. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | The Logic Analyzer will wait for the falling edge of the Rx signal to be triggered (corresponding to the start bit). | ||
+ | |||
+ | Run a single sweep on the Pattern Generator to send the first UART byte. | ||
+ | |||
+ | The result captured by the Logic Analyzer is presented in Figure 10. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | Analyzing the plot, the byte (ASCII code) corresponding to character " | ||
+ | |||
+ | The decoders available in Scopy allow visualization of the data bytes in ASCII format, including the Start Bit (denoted with " | ||
+ | |||
+ | Now, let's try sending multiple characters and see what happens with our application. | ||
+ | |||
+ | In the Pattern Generator instrument, under the "Data to Send" label, set the data bytes to " | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | On the Logic Analyzer, adjust the Time Base and Trigger Position accordingly to be able to see all of the transactions. (i.e. Time Base: 100us and Trigger Position: 300us) | ||
+ | |||
+ | Run Single sweep in The Logic Analyzer and then in the Pattern Generator. | ||
+ | |||
+ | The result captured by the Logic Analyzer is shown in Figure 12. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
+ | |||
+ | The EVAL-ADICUP3029 example program echoes received data bytes as they come in. As expected all the data bytes were received by the EVAL-ADICUP3029 board and sent back on Tx pin. | ||
+ | |||
+ | =====Conclusion===== | ||
+ | |||
+ | In addition to UART, the application includes a set of decoders covering a large number of communication protocols such as I2C, I2S, SPI, JTAG, and others, making ADALM2000 a powerful tool for analyzing and debugging digital signals. | ||
+ | |||
+ | ====Further Reading: | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[university: | ||
+ | * [[university: | ||