This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-scr [24 Jul 2017 16:10] – change amplitude value to peak-peak Antoniu Miclaus | university:courses:electronics:electronics-lab-scr [27 May 2022 21:00] (current) – [LATCH-UP] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======Activity: | + | ======Activity: |
=====Objective: | =====Objective: | ||
Line 103: | Line 103: | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | AWG1 should be configured as a sine wave with an amplitude of 10 V, zero offset and a frequency of 100 | + | AWG1 should be configured as a sine wave with an amplitude of 10 V peak-to-peak, zero offset and a frequency of 100 |
- | Hz. AWG2 should be configured as a square wave with an amplitude of 800 mV, 400 mV offset, a frequency | + | Hz. AWG2 should be configured as a square wave with an amplitude of 800 mV peak-to-peak, 400 mV offset, a frequency |
- | of 100 Hz and a duty cycle (symmetry) of 10%. 10% is the narrowest pulse width allowed by the Scopy | + | of 100 Hz. Be sure to run the two AWG channels synchronously. |
- | software. Be sure to run the two AWG channels synchronously. | + | {{ : |
+ | |||
+ | <WRAP centeralign> | ||
=====Procedure: | =====Procedure: | ||
Line 112: | Line 114: | ||
Trigger the scope on channel 1. While observing the input sine wave on scope channel 1 and the voltage | Trigger the scope on channel 1. While observing the input sine wave on scope channel 1 and the voltage | ||
across R< | across R< | ||
- | on the phase setting of AWG2 you should see something that looks similar to figure 3. You will notice | + | on the phase setting of AWG2 you should see something that looks similar to the figures below. You will notice |
that the voltage across R< | that the voltage across R< | ||
occurs and the SCR remains in the ON state until the input sine wave voltage crosses zero. | occurs and the SCR remains in the ON state until the input sine wave voltage crosses zero. | ||
- | |||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
Measure and report the voltage drop across the SCR when it is in the ON state and conducting current. How does this voltage compare to a conventional PN junction diode? | Measure and report the voltage drop across the SCR when it is in the ON state and conducting current. How does this voltage compare to a conventional PN junction diode? | ||
Line 152: | Line 158: | ||
Latch-up is a potentially destructive situation in which a parasitic SCR is triggered, shorting the | Latch-up is a potentially destructive situation in which a parasitic SCR is triggered, shorting the | ||
- | positive and negative supplies together. If current flow is not limited, electrical | + | positive and negative supplies together. If current flow is not limited, electrical |
occur. The classic case of latch-up occurs in CMOS output devices, in which the driver transistors and | occur. The classic case of latch-up occurs in CMOS output devices, in which the driver transistors and | ||
wells form a four layer PNPN SCR structure when one of the two parasitic base-emitter junctions is | wells form a four layer PNPN SCR structure when one of the two parasitic base-emitter junctions is | ||
- | momentarily forward biased during an overvoltage | + | momentarily forward biased during an over-voltage |
short between the V< | short between the V< | ||
Line 167: | Line 173: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
- | Proper design methods to reduce the possiblility | + | Proper design methods to reduce the possibility |
- | NMOS and PMOS devices and interposing highly doped regions | + | NMOS and PMOS devices and interposing highly doped regions |
these kinds of layout approaches attempt to lower the ß of either the vertical PNP or the lateral NPN | these kinds of layout approaches attempt to lower the ß of either the vertical PNP or the lateral NPN | ||
parasitic bipolar transistors to less than 1. Some of these methods also tend to lower the resistance of | parasitic bipolar transistors to less than 1. Some of these methods also tend to lower the resistance of | ||
Line 176: | Line 182: | ||
the SCR. | the SCR. | ||
- | **For Further Reading:** | + | <WRAP round download> |
+ | **Resources:** | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
- | http:// | + | =====The Programmable UJT (PUT)===== |
- | [[http:// | + | The Programmable unijunction transistor or PUT is a close relative of other four layer devices in the thyristor family. Its has a four layered construction just like the SCR and has three terminals named anode(A), cathode(K) and gate(G) again like the thyristors. Background and example circuits that use the PUT can be found in this [[:university: |
+ | |||
+ | **For Further Reading:** | ||
- | [[http://www.analog.com/ | + | [[http://en.wikipedia.org/wiki/ |
+ | [[adi> | ||
+ | [[adi>library/ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||