Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:courses:electronics:electronics-lab-nr [19 Dec 2018 10:50] – add Fritzing files Antoniu Miclaus | university:courses:electronics:electronics-lab-nr [25 Jun 2020 22:07] – external edit |
---|
====Testing supply headroom==== | ====Testing supply headroom==== |
| |
To test the headroom requirements for +V<sub>DD</sub>, disconnect the fixed positive power supply from +V<sub>DD</sub> and remove any supply decoupling capacitors. Be sure to turn off the power supplies before making any changes or additions to your breadboard. Now connect +V<sub>DD</sub> to AWG 1. Set AWG 1 to trapezium (trapezoid) waveform at 100 Hz. Set the amplitude to 5V with a 2.5V offset for a 0 to +5V swing. Connect scope channel 1 to the output of AWG1 and connect scope channel 2 to -V<sub>REF</sub> of the first example circuit at pin 14 of the OP482. Use the oscilloscope instrument in the XY mode, scope channel for X and scope channel 2 for Y. Start AWG 1 and turn on the fixed negative 5V power supply. Record the minimum +V<sub>DD</sub> voltage where -V<sub>REF</sub> starts to remain constant at -1.25V. | To test the headroom requirements for +V<sub>DD</sub>, disconnect the fixed positive power supply from +V<sub>DD</sub> and remove any supply decoupling capacitors. Be sure to turn off the power supplies before making any changes or additions to your breadboard. Now connect +V<sub>DD</sub> to AWG 1. Set AWG 1 to trapezium (trapezoid) waveform at 100 Hz. Set the amplitude to 5V peak-to-peak with a 2.5V offset for a 0 to +5V swing. Connect scope channel 1 to the output of AWG1 and connect scope channel 2 to -V<sub>REF</sub> of the first example circuit at pin 14 of the OP482. Use the oscilloscope instrument in the XY mode, scope channel for X and scope channel 2 for Y. Start AWG 1 and turn on the fixed negative 5V power supply. Record the minimum +V<sub>DD</sub> voltage where -V<sub>REF</sub> starts to remain constant at -1.25V. |
| |
To test the headroom requirements for -V<sub>SS</sub>, reconnect +V<sub>DD</sub> to the fixed positive power supply. Disconnect the fixed negative power supply from -V<sub>SS</sub> and remove any supply decoupling capacitors. Now connect -V<sub>SS</sub> to AWG 1. Set the amplitude to 5V with a -2.5V offset for a 0 to -5V swing. Start AWG 1 and turn on the fixed positive 5V power supply. Repeat your measurements of pins 14 of the OP482 recording the lowest value for -V<sub>SS</sub> where the reference voltage is constant. | To test the headroom requirements for -V<sub>SS</sub>, reconnect +V<sub>DD</sub> to the fixed positive power supply. Disconnect the fixed negative power supply from -V<sub>SS</sub> and remove any supply decoupling capacitors. Now connect -V<sub>SS</sub> to AWG 1. Set the amplitude to 5V peak-to-peak with a -2.5V offset for a 0 to -5V swing. Start AWG 1 and turn on the fixed positive 5V power supply. Repeat your measurements of pins 14 of the OP482 recording the lowest value for -V<sub>SS</sub> where the reference voltage is constant. |
| |
=====Directions Step 3:===== | =====Directions Step 3:===== |
Repeat the supply headroom tests you did in Step 2 for this configuration. Are there any differences? | Repeat the supply headroom tests you did in Step 2 for this configuration. Are there any differences? |
| |
| <WRAP round download> |
**Resources:** | **Resources:** |
* Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/neg_voltage_ref_bb | neg_voltage_ref_bb]] | * Fritzing files: [[downgit>education_tools/tree/master/m2k/fritzing/neg_voltage_ref_bb | neg_voltage_ref_bb]] |
| * LTspice files: [[downgit>education_tools/tree/master/m2k/ltspice/neg_voltage_ref_ltspice | neg_voltage_ref_ltspice]] |
| </WRAP> |
====For further reading:==== | ====For further reading:==== |
| |