This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-external-trigger [24 Jul 2017 16:18] – change amplitude value to peak-peak Antoniu Miclaus | university:courses:electronics:electronics-lab-external-trigger [14 Dec 2018 11:50] – add Fritzing files Antoniu Miclaus | ||
---|---|---|---|
Line 34: | Line 34: | ||
Waveform generator AWG1 should be set up as a triangle wave with a 8 Volt amplitude and 0 V offset and a frequency of 5 KHz. Set the horizontal and vertical scales of the scope to display at least one complete cycle of the input triangle waveform. Turn on the power supplies only after double checking your circuit connections. | Waveform generator AWG1 should be set up as a triangle wave with a 8 Volt amplitude and 0 V offset and a frequency of 5 KHz. Set the horizontal and vertical scales of the scope to display at least one complete cycle of the input triangle waveform. Turn on the power supplies only after double checking your circuit connections. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
=====Procedure: | =====Procedure: | ||
To start, set the scope trigger source to Channel 1, rising edge, with the level set to 0 V. You should see the rising edge of the triangle wave on channel 1 centered on the 0 time point along the horizontal axis. The rising edge of the digital output of the second inverter on channel 2 should occur at different times along the horizontal axis depending on the setting of the potentiometer, | To start, set the scope trigger source to Channel 1, rising edge, with the level set to 0 V. You should see the rising edge of the triangle wave on channel 1 centered on the 0 time point along the horizontal axis. The rising edge of the digital output of the second inverter on channel 2 should occur at different times along the horizontal axis depending on the setting of the potentiometer, | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
Now switch the scope trigger source to external 1 (T1 input) and repeat the sweep of R< | Now switch the scope trigger source to external 1 (T1 input) and repeat the sweep of R< | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
Now move the input of the first inverter to pin 8 of the AD8561. The 0 time point should now align with the falling edge of the input triangle wave. Again repeat the sweep of R< | Now move the input of the first inverter to pin 8 of the AD8561. The 0 time point should now align with the falling edge of the input triangle wave. Again repeat the sweep of R< | ||
Line 71: | Line 81: | ||
The second Inverter is made by connecting pin 2 to V< | The second Inverter is made by connecting pin 2 to V< | ||
+ | **Resources: | ||
+ | * Fritzing files: [[ https:// | ||