This is an old revision of the document!
The objective of this lab activity is to investigate a circuit to interface analog signals to the digital external trigger input(s) of the ADALM2000 module.
The ADALM2000 scope module is most often triggered from one of the analog input channels. This will display stable waveforms with the horizontal time scale ( align zero time point ) based on whichever channel is selected as the trigger source. It is sometimes desirable to trigger the display ( zero time point reference ) using a third signal from some other point in the circuit being tested. The ADALM2000 hardware provides two external digital inputs, T1 and T2, which can be selected as trigger inputs. Using these digital inputs the displayed waveforms will align ( set the zero time point ) with the rising edge of the applied signal. These are however digital inputs and only allow input voltages between 0 and +5V and have a fixed threshold voltage. In order to use these external trigger inputs with analog input signals, that is to say between -5 V and +5 V, a voltage comparator circuit along with a adjustable voltage source to set the trigger voltage level are needed. In this lab activity an example circuit will be explored
ADALM2000 Active Learning Module
Solder-less breadboard
Jumper wires
1 - AD8561 comparator ( or AD790 alternate with slightly different pinout )
1 - 74HC04 Hex CMOS inverter ( or CD4007 see Appendix )
3 - 1 KΩ resistors
1 - 1 megaΩ resistor
1 - 10 KΩ potentiometer
1 - 0.1 uF capacitor
1 - 0.0047 uF capacitor
Build the circuit shown in figure 1 on your solder-less breadboard. The AD8561 analog comparator has non-inverted (true) and inverted (complement) outputs. The input of the first inverter can be alternately connected to either the pin 7 output, for a rising edge, or the pin 8 output, for a falling edge trigger. Start with it connected to pin 7. The 74HC04 hex inverter is suggested but a CD4069 hex inverter may be substituted or the two inverters can be built using the CD4007 transistor array supplied in the Parts Kit ( see Appendix ).
The AD8561 has a very high bandwidth and will respond to any high frequency noise that might be present on the input signal. This will cause its output(s) to switch back and forth multiple times very quickly if the input signal is near the threshold voltage (VTH). This noise will cause the waveform displayed on the screen to jump or “jitter” back and forth and look unstable. Resistor R5 and capacitor C1 form a low pass filter and are inserted between the two inverter stages to reduce these very fast switching spikes. The time constant of this filter would be adjusted based on the nature of the signal being used as the external trigger.
Figure 1 Analog trigger circuit
Waveform generator AWG1 should be set up as a triangle wave with a 8 Volt amplitude and 0 V offset and a frequency of 5 KHz. Set the horizontal and vertical scales of the scope to display at least one complete cycle of the input triangle waveform. Turn on the power supplies only after double checking your circuit connections.
To start, set the scope trigger source to Channel 1, rising edge, with the level set to 0 V. You should see the rising edge of the triangle wave on channel 1 centered on the 0 time point along the horizontal axis. The rising edge of the digital output of the second inverter on channel 2 should occur at different times along the horizontal axis depending on the setting of the potentiometer, R3. Adjust R3 up and down from one end of its range to the other and observe where the rising edge of the pulse on channel 2 occurs with respect to the voltage (vertical axis) of the triangle wave at that time point.
Now switch the scope trigger source to external 1 (T1 input) and repeat the sweep of R3 from one end of its range to the other. You should be able to align the 0 time point anywhere along the rising edge.
Now move the input of the first inverter to pin 8 of the AD8561. The 0 time point should now align with the falling edge of the input triangle wave. Again repeat the sweep of R3 to confirm that you are able to align the 0 time point anywhere along the falling edge.
What is the purpose of the 1 megOhm resistor connected from the non-inverting input of the AD8561 to ground? What other components could you add to the input to allow input voltages beyond the +/- 5 volt power supply limits?
What methods, other than the RC filter, could be used to remove the noise jitter from the comparator? (Hint: see the For Further Reading section) Are there any advantages or disadvantages with using one method or the other?
Ask The Applications Engineer - High-speed comparators provide many useful circuit functions when used correctly.
Curing Comparator Instability with Hysteresis
Return to Activity Table of Contents.
Below is the schematic and pinout for the CD4007:
CD4007 CMOS transistor array pinout
As many as three individual inverters can be built from one CD4007 package. The simplest first one to configure as shown below is by connecting pins 8 and 13 together as the inverter output. Pin 6 will be the input. Be sure to connect pin 14 VDD to power and pin 7 VSS to ground.
The second Inverter is made by connecting pin 2 to VDD, pin 4 to VSS, pins 1 and 5 are connected together as the output and with pin 3 as the input. The third inverter is made by connecting pin 11 to VDD, pin 9 to VSS, pin 12 is the output and pin 10 is the input.