This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:alm1k:alm-lab-heart-rate-mon [25 Nov 2017 17:28] – [Materials] Doug Mercer | university:courses:alm1k:alm-lab-heart-rate-mon [14 May 2022 16:31] (current) – [Questions] Doug Mercer | ||
---|---|---|---|
Line 17: | Line 17: | ||
=====Background===== | =====Background===== | ||
- | A type of Heart Rate Monitor consists of an electronic circuit that monitors heartbeat by clipping onto a finger tip. It does this by shining light into or through your finger and measuring how much light is reflected or absorbed. This goes up and down as blood is pumped through your finger. For the operation as a optical heartbeat detector, a pair of IR LED and Phototransistor | + | A type of Heart Rate Monitor consists of an electronic circuit that monitors heartbeat by clipping onto a finger tip. It does this by shining light into or through your finger and measuring how much light is reflected or absorbed. This goes up and down as blood is pumped through your finger. For the operation as a optical heartbeat detector, a combination |
- | The voltage variations change with the heartbeat and are acquired from the collector of the phototransistor. The small signal obtained is used as input for the following circuit, providing an output signal as a heartbeat detector or monitor. | + | The voltage variations change with the heartbeat and are acquired from the collector of the photo transistor. The small signal obtained is used as input for the following circuit, providing an output signal as a heartbeat detector or monitor. |
In order to have a relevant output, the input signal is passed through multiple circuits: | In order to have a relevant output, the input signal is passed through multiple circuits: | ||
*Preamplifier - the output signal from the heartbeat measurement setup is decoupled through the series capacitor and amplified using a negative feedback resistor(R4). | *Preamplifier - the output signal from the heartbeat measurement setup is decoupled through the series capacitor and amplified using a negative feedback resistor(R4). | ||
*Low-Pass Filter - RC filter that cuts the high frequencies (noise). | *Low-Pass Filter - RC filter that cuts the high frequencies (noise). | ||
- | *[[university: | + | *[[university: |
- | *[[university: | + | *[[university: |
=====Materials===== | =====Materials===== | ||
+ | |||
+ | Select the following components from the ADALP2000 Analog Parts Kit. Note, the parts kit contains both OP-482 and OP-484 quad op-amps. They look very similar and are both in 14 pin DIP packages. The laser branding on the packages can be hard to read. Fortunately they share a common pinout so you will not damage them if you use the wrong one in this experiment by accident. The circuit will just not operate properly. | ||
+ | |||
+ | There are two black plastic devices with two leads in the kit that look almost exactly the same. One is the photo transistor and the other is a photo diode. The one with the slightly shorter leads should be the photo transistor. If you have a DMM with a diode test function handy you can verify which is the photo diode and which is the photo transistor (the photo diode will conduct in one direction and the photo transistor will not conduct in either direction) | ||
ADALM1000 Active Learning Module\\ | ADALM1000 Active Learning Module\\ | ||
Solder-less breadboard\\ | Solder-less breadboard\\ | ||
Jumper wires\\ | Jumper wires\\ | ||
- | 1 - OP484 precision rail-to-rail I/O op amp\\ | + | 1 - OP484 precision rail-to-rail I/O op amp (14 pin DIP package)\\ |
- | 1 - 100Ω resistor\\ | + | {{ : |
- | 1 - 220Ω resistor\\ | + | <WRAP centeralign> |
- | 1 - 470Ω resistor\\ | + | |
- | 1 - 1.5KΩ resistor\\ | + | Resistors are marked with color bands like this:\\ |
- | 1 - 10KΩ resistor\\ | + | {{ : |
- | 1 - 22KΩ resistor\\ | + | |
- | 1 - 47KΩ resistor\\ | + | Find resistors with the following color bands:\\ |
- | 2 - 1uF capacitor\\ | + | 1 - 100Ω resistor |
+ | 1 - 470Ω resistor | ||
+ | 1 - 1KΩ resistor | ||
+ | 1 - 1.5KΩ resistor | ||
+ | 1 - 10KΩ resistor | ||
+ | 1 - 20KΩ resistor | ||
+ | 1 - 47KΩ resistor | ||
+ | |||
+ | 2 - 1uF capacitors\\ | ||
+ | {{ : | ||
1 - 47uF capacitor\\ | 1 - 47uF capacitor\\ | ||
- | 1 - Infrared LED ( QED-123 )\\ | + | {{ : |
- | 1 - Infrared Transistor | + | |
- | 1 - Red LED | + | 1 - Infrared LED (QED-123) |
{{ : | {{ : | ||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | 1 - Infrared Transistor (QSD-123) the longer of the two leads is the collector and the shorter lead is the emitter.\\ | ||
{{ : | {{ : | ||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | 1 - Red LED | ||
+ | {{ : | ||
=====Directions===== | =====Directions===== | ||
- | On your solder-less breadboard construct the heartbeat monitor circuit as shown in figure 1. | + | On your solder-less breadboard construct the heartbeat monitor circuit as shown in figure 1. The values shown for the gain setting resistors R< |
+ | |||
+ | The collector load resistor R< | ||
{{ : | {{ : | ||
Line 60: | Line 81: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | The circuit uses quad OP484FPZ from the ADALP2000 Analog Parts Kit, the schematic design was implemented with three of the Precision Rail-to-Rail Operational Amplifiers. They operate from a single supply (+5V) from the ADALM1000 module. | + | The circuit uses the OP484FPZ |
====IR LED==== | ====IR LED==== | ||
Line 163: | Line 184: | ||
* Download: {{: | * Download: {{: | ||
</ | </ | ||
+ | **For further reading:** | ||
+ | |||
+ | [[wp> | ||
+ | [[wp> | ||
+ | |||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: |