The purpose of this activity is to investigate the forward and reverse current vs. voltage characteristics of a bipolar junction transistor (BJT) connected as a diode.
As in all the ALM labs we use the following terminology when referring to the connections to the M1000 connector and configuring the hardware. The green shaded rectangles indicate connections to the M1000 analog I/O connector. The analog I/O channel pins are referred to as CA and CB. When configured to force voltage / measure current -V is added as in CA-V or when configured to force current / measure voltage -I is added as in CA-I. When a channel is configured in the high impedance mode to only measure voltage -H is added as CA-H.
Scope traces are similarly referred to by channel and voltage / current. Such as CA-V , CB-V for the voltage waveforms and CA-I , CB-I for the current waveforms.
ADALM1000 Hardware Module
Solder-less Breadboard
1 - 470 Ω Resistor (or any similar value)
1 - small signal NPN transistor (2N3904)
The current vs. voltage characteristics of the base-emitter junction of an NPN transistor can be measured using the ALM1000 module and the following connections. Set up the breadboard with the channel A generator, CA-V, attached to one end of resistor R1. Connect the base and collector of Q1 to the opposite end of R1 as shown in the diagram. The emitter of Q1 is connected to ground. Connect channel B scope input, CB-H, to the base - collector node of Q1.
Figure 1 NPN diode connection diagram
The channel A generator should be configured for a 100 Hz triangle wave with a 5 volt Max and 0 volt Min. The channel A ammeter function (CA-I) measures the current in the resistor (and in the transistor). Scope channel B is connected to measure the voltage across the transistor. The current flowing through the transistor, can also be calculated as the voltage difference CA-V - CB-V math waveform divided by the resistor value (470 Ω for example).
Load the captured data in to a spreadsheet program like Excel and calculate the current. Plot the current ( measured and calculated ) vs. the voltage across the transistor (VBE). No current flows in the reverse direction. In the forward conduction region, the voltage, current relationship is logarithmic. If the current is plotted on a log scale the line should be straight.
Derive the mathematical expression for the current, IC, given the voltage across the transistor VBE?
The purpose of this activity is to investigate the reverse break down voltage characteristics of the emitter base junction of a bipolar junction transistor (BJT) connected as a diode.
1 - 100 Ω Resistor (or any similar value)
1 - small signal PNP transistor (2N3906)
4.5 volt battery ( three AA cells in series for example )
Set up the breadboard with the channel A generator output attached to one end of the series connected resistor 100 ? R1 and base and collector of Q1 as shown in figure 2. The emitter is connected to the negative 4.5 Volt fixed battery voltage. The channel B scope input, CB-H, is connected to the base - collector node. Scope trace CA-I measures the current through Q1. The PNP 2N3906 is chosen over the NPN 2N3904 because the PNP emitter base breakdown voltage is less than the +9.5 V max that can be generated using ALM1000 and the external 4.5V battery while the NPN's is likely to be higher than 10 V.
Figure 2 PNP Emitter Base Reverse breakdown configuration
The channel A generator should be configured for a 100 Hz triangle wave with 5 volt Max and 0 volt Min. Scope channel B is used to measure the voltage across the transistor. Both channels should be set to 0.5 V per division. The current flowing through the transistor is the current measured in channel A (CA-I) or the Math trace voltage difference between CA-V - CB-V divided by the resistor value (100 Ω).
The ALM1000 hardware power supply limits the maximum voltage available to 5 volts. The emitter base reverse breakdown voltage of many transistors is larger than this. In the configuration shown, voltages between 4.5 volts and 9.5 volts ( CA-V peak to peak swing + external battery voltage ) can be measured.
Capture the scope waveforms and export them into a spreadsheet program such as Excel. For the 2N3906 PNP used in the example, the breakdown voltage of the emitter base junction should be around 8.5 volts. Remember to add the 4.5 V offset from the external battery to your calculations. Be sure to measure the actual battery voltage for the most accurate measurements.
Disconnect the collector of Q1and leave it open. How does this change the breakdown voltage?
Now connect the collector to the emitter. How does this change the breakdown voltage?
Try measuring the NPN 2N3904 emitter base reverse breakdown voltage. You can also check the emitter base breakdown voltage for the two power transistors, TIP31 and TIP32, which are included in the Analog Parts Kit. Are they higher or lower than the PNP 2N3906 and is it lower than the +9.5 volts you can measure with this setup? If it is higher what could you change in the setup to allow you to measure higher breakdown voltages?
The purpose of this activity is to investigate a circuit configuration with smaller forward voltage characteristics than that of a bipolar junction transistor (BJT) connected as a diode.
1 - 1KΩ Resistor
1 - 150KΩ Resistor ( or 100KΩ in series with 47KΩ )
1 - small signal NPN transistor (2N3904)
1 - small signal PNP transistor (2N3906)
Set up the breadboard, as shown in figure 3, with the channel A generator attached to one end of the series connected resistor R1 and collector of NPN Q1 and the base of PNP Q2. The emitter of Q1 is connected to ground. The collector of Q2is connected to ground. The first end of Resistor R2 is connected to +5V. The second end of R2 is connected to the base of Q1 and the emitter of Q2. The channel B scope input, CB-H, is connected to the collector of Q1.
Figure 3 Configuration to lower effective forward voltage drop of diode
The channel A generator should be configured for a 100 Hz triangle wave with 5 volt Max and 0 volt Min. Scope channel B is used to measure the voltage across the transistor. The current flowing through the transistor is the current measured in channel A (CA-I) or the Math trace voltage difference between CA-V - CB-V divided by the resistor value (1 KΩ).
The turn on voltage of the “diode” is now about 100mV compared to 650mV for the simple diode connection in the first example. Plot the VCE of Q1 as CA-V is swept.
Could the collector of the PNP Q2 be connected to some other node such as a negative supply voltage?
And what would be the effect?
The value of R2 sets the current in Q2. What is the effect of increasing or decreasing the value of R2?
Now that we have seen a way to make VBE effectively smaller, the purpose of this activity is to make VBE larger. Larger forward voltage characteristics than that of a single bipolar junction transistor (BJT) connected as a diode.
2 - 2.2 KΩ Resistors
1 - 1 KΩ Resistor
1 - 5 KΩ Variable resistor, potentiometer
1 - small signal NPN transistor (2N3904)
Set up the breadboard, as shown in figure 4, with the channel A generator attached to one end of resistor R1. The emitter of Q1 is connected to ground. Resistors R2, R3 and R4 form a voltage divider with the wiper of potentiometer R3 connected to the base of Q1. The collector of Q1 is connected to the second end of R1 and the top of the voltage divider at R2. Scope channel B is connected to the collector of Q1.
Figure 4 VBE Multiplier configuration
The channel A generator should be configured for a 100 Hz triangle wave with 5 volt Max and 0 V Min. The input of scope channel B is used to measure the voltage across the transistor. The software should be configured to display CA-V and channel CB-V, the collector voltage of Q1. The current flowing through the transistor is the current measured in channel A (CA-I) or the Math trace voltage difference between CA-V - CB-V divided by the resistor value (1 KΩ).
Starting with the potentiometer R3 set at the middle of its range the voltage at the collector of Q2 should be about 2 times VBE. With R3 set to its minimum the voltage at the collector should be 9/2 (or 4.5) times VBE. With R3 set to its maximum the voltage at the collector should be 9/7 times VBE.
How does the voltage vs current characteristics of this VBE multiplier compare to those of a simple diode connected transistor?
Aside from the position of the potentiometer wiper, do the values of R2, R3 and R4 effect the shape of the I vs V curve? To arrive an answer try using values much larger and much smaller than those listed above.
Resources:
For Further Reading:
Return to ALM Lab Activity Table of Contents