You can find the results of your wiki search below. If you didn't find what you were looking for, you can create or edit the page named after your query with the appropriate button, or search the rest of Analog.com. If that doesn't work, try Google.
ote>
In general, a given reference design for an FMC board is deployed to just a few carriers, althoug... heck =====
<note>All ADI's FPGA Mezzanine Cards (FMC) are designed to respect all the specifications a... ired carrier card.</note>
There are two types of FMC connectors: LPC (Low Pin Count) and HPC (High Pin Count). In general, an FMC board is using the FMC connector type that has en
ripherals located on the prototyping board or the FMC IO board. \\
In HDL, these ports are named slight... rfaces, which are used as a control interface for FMC/HSMC devices. These SPI interfaces are controlled... s, buttons and/or LEDs, which can be found on the FMC board.
When some of these GPIOs are not used, th... that describes the behavior; here you define the FMC I/O pins, board-specific clock signals, timing co
├─ projects
│ ├ ad6676evb
│ ├ ad9467_fmc
│ ·
│ ├ common
│ ├ fmcomms2
│ ... ot necessarily mean that you can use it with your FMC board.
* **scripts**: In all cases, we are inte... , that means your FPGA board with that particular FMC board is not supported.
==== The library are str