This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:uc-drivers:microchip:ad7476 [01 Oct 2012 14:45] – created Dragos Bogdan | resources:tools-software:uc-drivers:microchip:ad7476 [22 Jul 2019 11:24] (current) – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{: | + | <WRAP round download 80%> |
- | * {{: | + | |
* {{: | * {{: | ||
- | * {{: | + | * {{: |
+ | * **AD74xx Driver: | ||
+ | * **PmodAD1 Demo for PIC32MX320F128H: | ||
+ | * **PIC32MX320F128H Common Drivers: | ||
+ | </ | ||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
Line 22: | Line 25: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * The AD7476 demonstration project for PIC32MX320F128H. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The AD7476 demonstration project for PIC32MX320F128H consists of three parts: the **AD74xx Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | A PmodAD1 has to be connected to the JE connector of Cerebot MX3cK development board. | + | A PmodAD1 has to be connected to the JE connector of Cerebot MX3cK development board in this particulary way: |
+ | PmodAD1 J1 connector Pin CS → Cerebot MX3cK JE connector Pin 1 | ||
+ | PmodAD1 J1 connector Pin D0 → Cerebot MX3cK JE connector Pin 3 | ||
+ | PmodAD1 J1 connector Pin CLK → Cerebot MX3cK JE connector Pin 4 | ||
+ | PmodAD1 J1 connector Pin GND → Cerebot MX3cK JE connector Pin 5 | ||
+ | PmodAD1 J1 connector Pin VCC → Cerebot MX3cK JE connector Pin 6 | ||
{{ : | {{ : | ||
+ | |||
+ | <WRAP round important round 80%> | ||
+ | \\ | ||
+ | * The reference voltage for the AD7476 is 3.3V. | ||
+ | \\ | ||
+ | </ | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following | + | The following |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | voltage? | Initiates a conversion and displays the captured | + | | voltage? | Initiates a conversion and displays the voltage |
- | | register? | Initiates a conversion and displays the raw data in decimal format. | | + | | register? | Initiates a conversion and displays the value from the register. | |
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | + | The following image shows a generic |
{{ : | {{ : | ||
Line 74: | Line 95: | ||
{{page>: | {{page>: | ||
- | ====== Digilent Cerebot MX3cK Quick Start Guide - Arduino | + | ====== Digilent Cerebot MX3cK Quick Start Guide - chipKIT Project |
- | This section contains a description of the steps required to run the AD7476 | + | This section contains a description of the steps required to run the AD7476 |
==== Required Hardware ==== | ==== Required Hardware ==== | ||
Line 90: | Line 111: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following commands were implemented in this version of AD7476 | + | Following commands were implemented in this version of AD7476 |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | |