Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sigmastudiov2:usingsigmastudio:scripting [24 Jun 2020 08:54] – links added John Josephresources:tools-software:sigmastudiov2:usingsigmastudio:scripting [15 Mar 2024 11:42] (current) – [SigmaStudio+ Scripting] Arpit Arora
Line 1: Line 1:
 +[[resources/tools-software/sigmastudiov2/usingsigmastudio|Click here to return back]]
  
 ====== SigmaStudio+ Scripting====== ====== SigmaStudio+ Scripting======
  
-As a startup guide, this page simply introduces to the Scripting functionality supported by SigmaStudio+ Application This uses Apache Thrift and RPC protocol in order to connect to the server application(SS+). +As a startup guide, this page simply introduces to the Scripting functionality supported by SigmaStudio+ ApplicationThis uses Apache Thrift and RPC protocol in order to connect to the server application(SS+). 
-An example solution(i.e., CSharp client in this case is also given along with the package to make the user understand basic actions that are available for Scripting. +An example (i.e., CSharp client/Python) is also given along with the package to make the user understand basic actions that are available for Scripting. Refer to [[:resources:tools-software:sigmastudiov2:tutorials:remoteexecute|Remote Execute]] for detailed example for client application 
-Available actions for SigmaStudio scripting:+ 
 +Available actions for SigmaStudioscripting:
 \\ \\
- 
- 
  
   - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/createnewproject|CreateNewProject]]   - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/createnewproject|CreateNewProject]]
   - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/saveproject|SaveProject]]   - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/saveproject|SaveProject]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/openproject|OpenExistingProject]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/addshape|AddShape]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/removeshape|RemoveShape]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/addconnection|AddConnection]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/removeconnection|RemoveConnection]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/moveshape|MoveShape]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/rotateshape|RotateShape]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/resizeshape|ResizeShape]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/link|Link]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/linkcompileconnect|LinkCompileConnect]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/linkcompiledownload|LinkCompileDownload]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/updateproperties|UpdateProperties]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/getallplugins|GetAllPlugins]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/getavailablecanvaselements|GetAvailableCanvas]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/getelementsinsidecanvas|GetCanvasElements]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/getproperties|GetProperties]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/export|Export]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/import|Import]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/getpluginproperties|GetPluginProperties]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/updatebooleanproperty|UpdateBooleanProperty]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/updatenumericproperty|UpdateNumericProperty]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/updatestringproperty|UpdateStringProperty]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/updatelistproperty|UpdateListProperty]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/exportpreset|ExportPreset]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/importpreset|ImportPreset]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/execute|Execute]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/read|Read]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/loadshape|LoadShape]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/saveshape|SaveShape]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/getcapture|GetCaptureViewEntries]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/clearcapture|ClearCaptureViewEntries]]
 +  - [[resources/tools-software/sigmastudiov2/usingsigmastudio/scripting/updatelabel|UpdateLabel]]
 +\\
 +==== Scripting.Thrift====
  
-1 list<string> CreateNewPorject(1: string projectName)\\ +     This file is given out for the user to generate files in a specific language with the help of commands as given in Apache thrift startup guide [[https://thrift.apache.org/tutorial/]].   
-2 list<string> SaveProject(1: string filePath)\\ +\\
-3 list<string> OpenExistingProject(1: string filePath)\\ +
-4 list<string> AddShape(1: string parentUid, 2: string shapeFullName, 3: Position newPosition)\\ +
-5 list<string> RemoveShape(1: string parentUid, 2: string shapeUid)\\ +
-6 list<string> AddConnection(1: string parentUid, 2: string channelFullName, 3: string sourceUid, 4:string targetUid, 5: string sourcePinType, 6: string targetPinType, 7: string sourcePinName, 8: string targetPinName)\\ +
-7 list<string> RemoveConnection(1: string parentUid, 2: string channelUid, 3: string linkUid)\\ +
-8 list<string> MoveShape(1: string shapeUid, 2: Position newPosition)\\ +
-9 list<string> RotateShape(1: string shapeUid, 2: Position newPosition, 3: double newAngle)\\ +
-10 list<string> ResizeShape(1: string shapeUid, 2: Position newPosition, 3: Size newSize)\\ +
-11 list<string> Link()\\ +
-12 list<string> LinkCompileConnect()\\ +
-13 list<string> LinkCompileDownload()\\ +
-14 list<string> UpdateProperties(1: string elementUid, 2: string propertyName, 3: string propertyType, 4: string propertyValue) +
-15 list<string> GetAllPlugins(1: string interfaceType) +
-16 list<string> GetAvailableCanvasElements() +
-17 list<string> GetElementsInsideCanvas(1: string parentUid) +
-18 list<string> GetProperties(1: string elementUid) +
- +
-SdkScripting.Thrift file +
- This file is given out for the user to generate files in a specific language with the help of commands as given in Apache thrift startup guide.  +
  
-The example client solution lets the user verify all the actions in simple steps. 
-1. Choose the action to perform(by entering the serial number given against any action) 
-2. Under each of the action chosen, the console application displays every step involved to achieve full result. 
-3. If the user has access to UI, all the steps can be observed on the SigmaStudio application UI. 
-4. Press enter after each step to go onto the execution of the next step.  
-5. Result/Error can be observed instantly on the console application. 
-6. A message, “Would you like to continue? Y/N  ” appears on the app once the chosen action is successfully completed. 
  
resources/tools-software/sigmastudiov2/usingsigmastudio/scripting.txt · Last modified: 15 Mar 2024 11:42 by Arpit Arora