Wiki

This version (18 Nov 2021 08:09) was approved by John Joseph.The Previously approved version (16 Nov 2021 04:20) is available.Diff

Click here to return back

SigmaStudio+ Scripting

As a startup guide, this page simply introduces to the Scripting functionality supported by SigmaStudio+ Application. This uses Apache Thrift and RPC protocol in order to connect to the server application(SS+). An example (i.e., CSharp client/Python) is also given along with the package to make the user understand basic actions that are available for Scripting. Refer to Remote Execute for detailed example for client application.

Available actions for SigmaStudio+ scripting:


Scripting.Thrift

This file is given out for the user to generate files in a specific language with the help of commands as given in Apache thrift startup guide https://thrift.apache.org/tutorial/.

resources/tools-software/sigmastudiov2/usingsigmastudio/scripting.txt · Last modified: 16 Nov 2021 09:08 by Nikhin Shetty