This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:usingsigmastudio:scripting:openproject [24 Jun 2020 12:15] – created Krithika Manchale | resources:tools-software:sigmastudiov2:usingsigmastudio:scripting:openproject [15 Nov 2021 08:42] – Nikhin Shetty | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | [[resources/ | ||
+ | |||
=====Open Existing Project===== | =====Open Existing Project===== | ||
- | // | + | |
- | This takes in one argument(filePath) and allows the user to open a SigmaStudio project in the given filepath. | + | OpenExistingProject |
\\ | \\ | ||
+ | |||
===API=== | ===API=== | ||
< | < | ||
- | list< | + | SSPResult |
</ | </ | ||
\\ | \\ | ||
===Arguments==== | ===Arguments==== | ||
- | - filePath- The path along with the file name of the project which has to be opened in the SigmaStudio application. | + | - filePath- The path along with the file name of the project which has to be opened in the SigmaStudio+ application. |
\\ | \\ | ||
===Result=== | ===Result=== | ||
- | “The open project was successful” | + | SSPResult contains ' |
+ | -IsSuccess is ' | ||
+ | -Message contains the Success/ | ||
\\ | \\ | ||
\\ | \\ | ||
- | ===Error==== | ||
- | Displays the error msg as obtained by the Server application if any. | ||
- | |||
- |