Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:tools-software:sigmastudiov2:targetintegration:targetapplication:mcsupport [29 Jun 2020 07:29] – created Sreesha Y Mresources:tools-software:sigmastudiov2:targetintegration:targetapplication:mcsupport [27 Sep 2023 08:48] (current) – Minor corrections John Joseph
Line 2: Line 2:
 \\ \\
 =====Microcontroller Mode Support===== =====Microcontroller Mode Support=====
-In microcontroller mode, the Target Framework shall process the incoming audio data based on the exported set of code and parameters from SigmaStudio+. The ARM core of ADSP-SC5xx processor acts as a microcontroller, downloading the SMAP, SSn code and parameters on to the SHARC cores of ADSP-SC5xx.+In microcontroller mode, the Target Framework shall process the incoming audio data based on the exported set of code and parameters from SigmaStudio+. The ARM core of ADSP-SC5xx processor acts as a microcontroller, downloading the SMAP, SS+ code and parameters on to the SHARC cores of ADSP-SC5xx. Example micro controller mode applications are available in "C:\Analog Devices\SigmaStudioPlus-Relx.y.z\Target\Examples\DemoUc" folder.
 \\ \\
 \\ \\
-A utility is provided with the package by which the exported code and parameters by SigmaStudio+ can be converted into a ‘C’ compiler readable form. This utility create arrays of SMAP, SS+ code and parameters as part of a ‘C’ file which can directly be included in the SigmaStudio+ ARM application for ADSP-SC5xx.+A utility is provided with the package using which the code and parameters exported by SigmaStudio+ can be converted into a ‘C’ source files. This utility creates arrays of SMAP, SS+ code and parameters as part of a ‘C’ file which can be directly included in the SigmaStudio+ ARM application for ADSP-SC5xx. The export param utility is available in "C:\Analog Devices\SigmaStudioPlus-Relx.y.z\Target\Utilities\ExportCodeParam" folder. 
 + 
 +Please find the steps to export the schematic source files to use with micro controller application: 
 +  * Open SigmaStudio+, design the schematic application and compile the schematic. 
 +  * Upon successful compilation of schematic use "Export System Files" option to generate schematic export files.\\ 
 +{{:resources:tools-software:sigmastudiov2:targetintegration:targetapplication:export_system_files.png?400|}}\\ 
 +  * Copy the "ExportCodeParam.exe" utility available in installation package to the folder where the schematic export files are generated. 
 +  * Open Windows Command Prompt and change the working directory to this folder. 
 +  * Run the utility as below: 
 +ExportCodeParam.exe <SWC/NWC> <ExportName> <SchematicName> <ProcessorFamily>\\ 
 +example:\\  
 +//ExportCodeParam.exe "SWC" "Example" "DiffDXESchematic_1" “SC5xx” //\\ 
 +or \\ 
 +//ExportCodeParam.exe "SWC" "Example" "DiffDXESchematic_1" “215xx” //\\ 
 + 
 +This generates C source file and header file in the same folder. This utility must  
 +be run multiple times corresponding to the number of schematics within the  
 +core. Use the generated schematic source files to micro controller mode application and rebuild the application.\\ 
 + 
 +<note>The schematic source files should be regenerated when there is change in target application and/or SigmaStudio+ schematic.</note>
 \\ \\
resources/tools-software/sigmastudiov2/targetintegration/targetapplication/mcsupport.txt · Last modified: 27 Sep 2023 08:48 by John Joseph