In microcontroller mode, the Target Framework shall process the incoming audio data based on the exported set of code and parameters from SigmaStudio+. The ARM core of ADSP-SC5xx processor acts as a microcontroller, downloading the SMAP, SS+ code and parameters on to the SHARC cores of ADSP-SC5xx.
A utility is provided with the package by which the exported code and parameters by SigmaStudio+ can be converted into a ‘C’ compiler readable form. This utility create arrays of SMAP, SS+ code and parameters as part of a ‘C’ file which can directly be included in the SigmaStudio+ ARM application for ADSP-SC5xx.