Prototype
ADI_SS_COMM_RESULT adi_ss_comm_Packetize(ADI_SS_COMM_HANDLE hSSComm, ADI_SS_COMM_BACKCH_INFO *pBkChInfo, uint32_t *pPacketSzInWords )
Description
This API packetizes the back-channel data for transmission..
Parameters
Name: pPacketSzInWords Type: uint32_t Direction: Output Description: Pointer holding the size of the packet in words. Name: pBkChInfo Type: ADI_SS_COMM_BACKCH_INFO Direction: Input Description: Pointer to backchannel information structure. Name: hSSComm Type: ADI_SS_COMM_HANDLE Direction: Output Description: Handle to communication component instance \\
Return value
An error code of type ADI_SS_COMM_RESULT is returned.
• ADI_SS_COMM_SUCCESS : Communication init successful.
• ADI_SS_COMM_FAILED : Communication init failed due to general error.