This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:releaseinfo [18 Nov 2021 08:11] – John Joseph | resources:tools-software:sigmastudiov2:releaseinfo [15 Mar 2024 14:28] (current) – updated for SS+ 2.2.0 John Joseph | ||
---|---|---|---|
Line 2: | Line 2: | ||
\\ | \\ | ||
======Release Information====== | ======Release Information====== | ||
+ | =====2.2.0===== | ||
+ | ===Features=== | ||
+ | * Support for Pitch Shifter module for ADSP-SC5xx family of processors | ||
+ | * Link Compile Connect feature. | ||
+ | * Provision to configure export files naming convention. | ||
+ | * Enhances sequence window operations. Refer to sequence window wiki page for more information | ||
+ | * Misc. Features | ||
+ | * Provision to store the output links of a module and restore them to another module. | ||
+ | * Multiple notification control. | ||
+ | * Highlights selected link between two modules in a different color compared to others. | ||
+ | * Enhancements to table control. | ||
+ | * Logging feature for output and capture window. | ||
+ | * More detailed compilation result in output window | ||
+ | |||
+ | ===Bug Fixes=== | ||
+ | * Improves hierarchy board tool tip between connections. | ||
+ | * Selection of modules to be retained after copy paste operation. | ||
+ | * Addresses sequence window issues for I2C protocol with respect to data width field. | ||
+ | * Corrects A2B tab names reverting to old labels. | ||
+ | * Allows expansion and text trimming on Data column of capture window. | ||
+ | * Addresses copy, paste issues related to IO modules. | ||
+ | * Addresses generic undo, redo related issues. | ||
+ | * Ensures shape labels are unique. | ||
+ | * Migrates SigmaDSP configurations from SigmaStudio completely to SigmaStudio+. | ||
+ | * Addresses graphical parametric filter modules issues. | ||
+ | * Addresses generic alias pin issues | ||
+ | \\ | ||
+ | =====2.1.0===== | ||
+ | ===Features=== | ||
+ | * Support for ADSP-SC596 and ADSP-SC598 | ||
+ | * Provision to define new standard platforms using existing platforms | ||
+ | * Additional APIs supported in scripting interface | ||
+ | * Lock any platform/ | ||
+ | * Migration of SigmaStudio A2B projects to SigmaStudio+ | ||
+ | * Misc. Features | ||
+ | * Network bus length modification from the system view | ||
+ | * Context menu enhancements for ease of access of canvas and settings window | ||
+ | * Support for multiple communication protocol between communication device and platform | ||
+ | * Auto scroll while expanding in project window and toolbox entries | ||
+ | * Double click on a SigmaStudio+ project file to launch SigmaStudio+ and load the project | ||
+ | |||
+ | ===Bug Fixes=== | ||
+ | * Added Copy/Paste functionality in the system level and addressed other Copy/Paste issues | ||
+ | * Addressed distortions/ | ||
+ | * Addressed Save Shape and Load Shape issues | ||
+ | * Addressed pin related issues while closing and reopening of projects | ||
+ | * Addressed issues related to Undo-Redo of platforms | ||
+ | * Addressed issues in Thrift scripting APIs | ||
+ | * Addressed issues in SigmaStudio project migration | ||
+ | * Addressed linking and connection issues in Alias pin and Hierarchy boards | ||
+ | * Addressed slow response or crash while opening a canvas with large number of shapes and connectors | ||
+ | * Addressed the Update manager failure under certain networks | ||
+ | * Addressed application freeze issue while performing copy-paste or move shape operations | ||
+ | * Addressed issues related to inconsistent update on Project tree view or Tab header while editing the shape label | ||
+ | * Fix in SPORT Configuration while updating the processor | ||
+ | * Addressed compilation and migration issue on non-English language machines | ||
+ | * Addressed the issue of not able to close or move undocked windows on top of application title bar | ||
+ | * Miscellaneous fixes in module UI | ||
+ | \\ | ||
+ | =====2.0.0===== | ||
+ | ===Features=== | ||
+ | * Support for Networks and Network View | ||
+ | * Provision to store multiple alternate canvases and set one of the canvases as the active canvas for processing | ||
+ | * Enhanced project navigation | ||
+ | * Misc. Features | ||
+ | * Migration of ADAU145x/ | ||
+ | |||
+ | ===Bug Fixes=== | ||
+ | * TCPIP readback for ADSP-SC5xx/ | ||
+ | * Misc. fixes in ADAU145x/ | ||
+ | * Fixes in checksum, self-boot features | ||
+ | * Misc. user interface improvements | ||
+ | \\ | ||
+ | =====1.3.0 Eval===== | ||
+ | ===Features=== | ||
+ | * Support for ADSP-21593 and ADSP-SC594 processors | ||
+ | * Support for S/PDIF transmitter in default framework | ||
+ | * Undo-Redo Window | ||
+ | * Register read option in SigmaDSP Register Windows | ||
+ | * Addins Browser Window to add Plugins | ||
+ | * Integrated Examples | ||
+ | * Misc. Features | ||
+ | * Zoom-in/out supported in settings window | ||
+ | * Provision to reset and disable shape resize | ||
+ | * Auto save and restore unsaved changes | ||
+ | * Port configuration for scripting | ||
+ | * Ctrl+ Drag option to create a copy of shape | ||
+ | |||
+ | ===Bug Fixes=== | ||
+ | * Enhancements in capture and sequence windows | ||
+ | * Fixes in hierarchy board creation | ||
+ | * Fix in I2C register read | ||
+ | * Fix in Address Abstraction Metadata file | ||
+ | * Fix in communication check for SigmaDSP | ||
+ | * Enhancements to Alias Pin | ||
+ | * Enhancements to Copy-Paste operation | ||
+ | \\ | ||
=====1.2.0 Eval===== | =====1.2.0 Eval===== | ||
===Features=== | ===Features=== |