This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:tools-software:sigmastudiov2:modules:sources:vco [27 Feb 2020 06:12] – [Usage] Krithika Manchale | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | [[resources/ | ||
+ | ====== Voltage Controlled Oscillator ====== | ||
+ | \\ | ||
+ | {{: | ||
+ | ===== Description ===== | ||
+ | \\ | ||
+ | The Voltage Controlled Oscillator block, typically used for modulation applications. Takes the control input and generates a sine tone at particular frequency. | ||
+ | ===== Usage ===== | ||
+ | \\ | ||
+ | The input to the control pin could be varied from 0 to 1. VCO linearly interpolates its derived value into frequency from 0Hz (when input is 0) to FS/2(when input is 1). Where FS is the sampling frequency. | ||
+ | If the input applied is greater than 1, the derived output value will fold back to frequencies below fs/2. | ||
+ | ===== Targets Supported ===== | ||
+ | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | ||
+ | |VCO| Yes | Yes|Yes| Yes| | ||
+ | |||
+ | ===== Pins ===== | ||
+ | ==== Input ==== | ||
+ | ^Name^Type^Description^ | ||
+ | |ControlVoltage|Control|Controls the frequency of the sinetone| | ||
+ | |||
+ | ==== Output ==== | ||
+ | ^Name^Type^Description^ | ||
+ | |OscillatorOutput|Control|Output channel 0| | ||
+ | |||
+ | ===== Configurable Parameters ===== | ||
+ | No Configurable parameters | ||
+ | |||
+ | ===== DSP Parameters ===== | ||
+ | No DSP parameters | ||