This is an old revision of the document!
Click here to return to the Source page
The Voltage Controlled Oscillator block, typically used for modulation applications. Takes the control input and generates a sine tone at particular frequency.
The input to the control pin could be varied from 0 to 1. VCO linearly interpolates its derived value into frequency from 0Hz (when input is 0) to FS/2(when input is 1). Where FS is the sampling frequency.
If the input applied is greater than 1, the derived output value will fold back to frequencies below fs/2.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
VCO | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
ControlVoltage | Control | Controls the frequency of the sinetone |
Name | Type | Description |
---|---|---|
OscillatorOutput | Control | Output channel 0 |
No Configurable parameters
No DSP parameters