This shows you the differences between two versions of the page.
Next revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:inputoutput:output [13 Jan 2020 13:25] – created Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:inputoutput:output [06 May 2021 07:54] – Prasad Kamath | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== Output ====== | ====== Output ====== | ||
+ | \\ | ||
+ | {{: | ||
===== Description ===== | ===== Description ===== | ||
The Output block routes signals to the hardware' | The Output block routes signals to the hardware' | ||
+ | \\ | ||
===== Usage ===== | ===== Usage ===== | ||
Using the drop-down list, select the output channel to associate with a particular block. | Using the drop-down list, select the output channel to associate with a particular block. | ||
Line 9: | Line 12: | ||
The hardware outputs for a particular processor are limited. While designing you can see the number of outputs that are still available from the HWOutputs item of the Resources window. | The hardware outputs for a particular processor are limited. While designing you can see the number of outputs that are still available from the HWOutputs item of the Resources window. | ||
+ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^Name^ADSP-214xx^ADSP-215xx/ |
- | |Output| Yes | Yes|Yes| Yes| | + | |------------------|------------------------|--------------------------------------|----------------------------------| |
+ | |Output| Block & Sample| Block & Sample| Sample| | ||
+ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | |--------------------------------|-------------------------------------------------------|-------------------------------------------------------------------| | ||
|input0|Audio|Outputs the audio to the hardware pin| | |input0|Audio|Outputs the audio to the hardware pin| | ||
+ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | |--------------------------------|----------------------|--------------------------------|----------------------------------------| | ||
+ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
No DSP Parameters | No DSP Parameters | ||
+ | \\ | ||