Wiki

This version (18 May 2021 09:01) was approved by John Joseph.The Previously approved version (07 May 2021 14:33) is available.Diff

Click here to return to the IO page

Interface Write



Description


The Interface Write block sends signals from the schematic to an interface output register.


Usage


Each block is associated with only one interface register; select the appropriate one from the drop-down menu.

Observe that as you drag more blocks to your schematic, your number of interfaces available decreases.

Note: This block is only available for DSPs with GPIOs or auxiliary ADC.



Targets Supported

NameADSP-214xxADSP-215xx/ADSP-SC5xxADAU145x/1456x
—————————————-——————————————————————————————--——————————————-
Interface Write Not supported Not supported Sample


Pins

Input

NameTypeDescription
————————--———————————————————————-
Input Logic Interface write input channel


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
—————————————- ———————- ————————————- —————————————-
SelectedIFIPChannelINTFACE_0 INTFACE_0 to INTFACE_7 Selects the Interface Read channel


DSP Parameters

Not applicable

DSP Parameter Computation

Not applicable

resources/tools-software/sigmastudiov2/modules/inputoutput/interfacewrite.txt · Last modified: 12 May 2021 13:42 by Prasad Kamath