Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:tools-software:sigmastudiov2:modules:inputoutput:digmicinput [19 Mar 2021 15:26] – created Prasad Kamathresources:tools-software:sigmastudiov2:modules:inputoutput:digmicinput [13 May 2021 10:24] (current) – [Targets Supported] Prasad Kamath
Line 1: Line 1:
 +[[resources/tools-software/sigmastudiov2/modules/inputoutput|Click here to return to the IO page]]
 [[resources/tools-software/sigmastudiov2/modules/inputoutput|Click here to return to the IO page]] [[resources/tools-software/sigmastudiov2/modules/inputoutput|Click here to return to the IO page]]
 ====== Digital Microphone Input ====== ====== Digital Microphone Input ======
 +\\
 +{{:resources:tools-software:sigmastudiov2:modules:inputoutput:digital_mic_ssp.jpg?nolink&150|}}
 +\\
 +===== Description =====
 +The Digital Microphone Input block receives input from the hardware's microphone input pins and makes it available in the schematic design.
 +\\
 +===== Usage =====
 +Check the block for the input channel(s) you with to enable. Un-check the box disable an input channel. The pin will turn blue when an input is enabled and grey when disabled. The default block has two pins enabled, for stereo connection.
 +\\
 +===== Targets Supported =====
 +^Name^ADSP-214xx^ADSP-215xx/ADSP-SC5xx ^ADAU145x/ADAU146x^
 +|-----------------------------------|----------------------------|-------------------------------------------|--------------------------------|
 +|Digital Microphone Input| Block & Sample| Block & Sample | Sample |
 +\\
 +===== Pins =====
 +==== Output ====
 +^Name^Type^Description^
 +|-------------------------------|-------------------------------------|-----------------------------|
 +|Output0|Audio|Mic Output channel 0|
 +|Output1|Audio|Mic Output channel 1|
 +\\
 +===== Configurable Parameters =====
 +\\
 +Not applicable
 +\\
 +===== DSP Parameters =====
 +No DSP Parameters
 +\\
 +
resources/tools-software/sigmastudiov2/modules/inputoutput/digmicinput.1616163995.txt.gz · Last modified: 19 Mar 2021 15:26 by Prasad Kamath