This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:inputoutput:asrcinput [06 May 2021 12:32] – Prasad Kamath | resources:tools-software:sigmastudiov2:modules:inputoutput:asrcinput [12 May 2021 13:24] (current) – [Input] Prasad Kamath | ||
---|---|---|---|
Line 2: | Line 2: | ||
====== ASRC Input====== | ====== ASRC Input====== | ||
\\ | \\ | ||
- | {{: | + | {{: |
{{: | {{: | ||
===== Description ===== | ===== Description ===== | ||
- | The ASRC Input blocks route signals between the schematic design and the hardwares | + | The ASRC Input blocks route signals between the schematic design and the hardware |
< | < | ||
Line 14: | Line 14: | ||
* Every ASRC Output must have its input connected, else there will be errors on compilation. | * Every ASRC Output must have its input connected, else there will be errors on compilation. | ||
- | * To change the ASRC input' | + | * To change the ASRC input' |
- | * | + | |
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
^Name^ADSP-214xx^ADSP-215xx/ | ^Name^ADSP-214xx^ADSP-215xx/ | ||
- | |------------------|------------------------|--------------------------------------|----------------------------------| | + | |-------------------------|------------------------|--------------------------------------|----------------------------------| |
- | |ASRC Output| Not available | Not available | Sample| | + | |ASRC Input| Not available | Not available | Sample| |
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
- | ==== Input ==== | + | ==== Output |
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | |--------------------------------|-------------------------------------------------------|-------------------------------------------------------------------| | + | |--------------------------------|--------------------------------------------------|-------------------------------------------------------------------| |
- | |Output|Audio|Outputs the audio to the hardware | + | |Output|Audio|Outputs the asrc audio to the pin| |
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
Line 35: | Line 34: | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
^Parameter Name^Description^ADAU145x/ | ^Parameter Name^Description^ADAU145x/ | ||
- | | ----------------------------- | --------------------------------------------------------------------------------------------------- |----------------------------------------------------- | | + | | ----------------------------- | ------------------------------------------------------------------- |----------------------------------------------------- | |
- | |gain|gain to be applied to input channel|Fixed 8.24| | + | |gain|gain to be applied to input channel|FixPoint8d24| |
\\ | \\ |