Wiki

This version (18 May 2021 09:01) was approved by John Joseph.The Previously approved version (06 May 2021 13:04) is available.Diff

Click here to return to the IO page

ASRC Input


Description

The ASRC Input blocks route signals between the schematic design and the hardware ASRCs (Asynchronous Sample Rate Converters).

These blocks are only available for use with DSPs that have integrated ASRCs.


Usage

Use the input block's check boxes to enable or disable particular inputs.

  • Every ASRC Output must have its input connected, else there will be errors on compilation.
  • To change the ASRC input's Sampling Rate , Right-click the block name and select Set Sampling Rate, which brings up the Sampling Rate window (default is 48 kHz).


Targets Supported

NameADSP-214xxADSP-215xx/ADSP-SC5xxADAU145x/ADAU146x
————————-————————————————————--———————————-
ASRC Input Not available Not available Sample


Pins

Output

NameTypeDescription
——————————--————————————————--——————————————————————-
OutputAudioOutputs the asrc audio to the pin


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
——————————--———————-——————————--—————————————-
Gain1.00 to 127.999 Gain to be applied to input


DSP Parameters

Parameter NameDescriptionADAU145x/ADAU146x
—————————-- ——————————————————————- —————————————————--
gaingain to be applied to input channelFixPoint8d24


DSP Parameter Computation

gain= Gain

resources/tools-software/sigmastudiov2/modules/inputoutput/asrcinput.txt · Last modified: 12 May 2021 13:24 by Prasad Kamath