This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:gain:singleslewextvol [02 Mar 2020 07:17] – [Single Slew External Volume] Sreesha Y M | resources:tools-software:sigmastudiov2:modules:gain:singleslewextvol [06 May 2021 18:24] (current) – [Configurable Parameters] Nikhin Shetty | ||
---|---|---|---|
Line 2: | Line 2: | ||
====== Single Slew External Volume ====== | ====== Single Slew External Volume ====== | ||
\\ | \\ | ||
- | {{: | + | {{: |
===== Description ===== | ===== Description ===== | ||
The Single Slew Ext Vol block controls level of the signal through external pin. Such capability would be appropriate for an application like external control communication to ab 8-10 bit ADC. | The Single Slew Ext Vol block controls level of the signal through external pin. Such capability would be appropriate for an application like external control communication to ab 8-10 bit ADC. | ||
Line 10: | Line 10: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |Single Slew Ext Vol| Yes | Yes|Yes| Yes| | + | | ------------------------------------------------------------ | -------------------- | -------------------------------- | ---------------------------- | |
+ | |Single Slew Ext Vol| B/S | B/S | S | | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | |------------------------------|------------------------------------------------------------|------------------------------| | ||
|ControlInput|Control|Controls the signal level of output| | |ControlInput|Control|Controls the signal level of output| | ||
- | |Input0|Audio|Input channel | + | |Input <fc # |
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | |Output0|Control|Output channel | + | |------------------------------|------------------------------------------------------------|------------------------------| |
+ | |Output <fc # | ||
+ | Note: | ||
+ | * <fc # | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | |SlewRate(StepSize)|12|1 to 23|Controls the transtion | + | |------------------------------|-------------------------|--------------------------------------|----------------------------------------------------------| |
- | |SlewType|RC|RC, | + | |SlewRate(StepSize)|12|1 to 23|Controls the transition |
- | |NumChannels|1|20|Num of input and output channels.Change in this value requires re-compilation| | + | |SlewType|RC|RC, |
+ | |SlewType1|Linear Slew| NA |Slew type. Applicable to HW slew modules| | ||
+ | |SlewType2|Linear Slew| NA |Slew type. Applicable to HW slew modules| | ||
+ | |Index1|8|0 to 15|Slew rate which scales the Slew value| | ||
+ | |Index2|8|0 to 15|Slew rate which scales the Slew value| | ||
+ | |NumChannels|1|20|Num of input and output channels .Change in this value requires re-compilation| | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
^Parameter Name^Description^ADSP-214xx/ | ^Parameter Name^Description^ADSP-214xx/ | ||
- | |SlewRate|Controls the transtion time of signal from one level to another level|Float| | + | | ---------------------------------------- | -------------------------------------------------------------------------------- | ---------------------------------------- | ---------------------------- | |
+ | |SlewRate|Controls the transtion time of signal from one level to another level| Float |NA| | ||
+ | |slew_mode|Controls the transtion time of signal from one level to another level| NA| Integer32 | ||
\\ | \\ | ||
===== DSP Parameter Computation ===== | ===== DSP Parameter Computation ===== | ||
SlewRate | SlewRate | ||
\\ | \\ |