This is an old revision of the document!
Click here to return to the Gain page
The Single Slew Ext Vol block controls level of the signal through external pin. Such capability would be appropriate for an application like external control communication to ab 8-10 bit ADC.
This block has text filed to specify the slew rate for smooth transition from one level of the signal to another level.slew rate is configurable from 1 to 23. Signal transition from one level to another level is faster when slew rate value is low and Signal transition from one level to another level is slower when slew rate value is high.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Single Slew Ext Vol | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
ControlInput | Control | Controls the signal level of output |
Input0 | Audio | Input channel 0 |
Name | Type | Description |
---|---|---|
Output0 | Control | Output channel 0 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
SlewRate(StepSize) | 12 | 1 to 23 | Controls the transtion time of signal from one level to another level |
SlewType | RC | RC,DB(only in Block) | Allows to select the slew type for algorithm. Change in slewType requires re-compilation |
NumChannels | 1 | 20 | Num of input and output channels.Change in this value requires re-compilation |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
SlewRate | Controls the transtion time of signal from one level to another level | Float |
SlewRate = 2^(-1*StepSize)