This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:gain:gainenvelope [07 May 2021 07:58] – [DSP Parameter Computation] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:gain:gainenvelope [07 May 2021 09:23] (current) – [Output] Nikhin Shetty | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== Gain Envelope ====== | ====== Gain Envelope ====== | ||
- | \\ | ||
{{: | {{: | ||
\\ | \\ | ||
Line 17: | Line 16: | ||
- Generic Gain Envelope | - Generic Gain Envelope | ||
- Gain Envelope EndlessLoop | - Gain Envelope EndlessLoop | ||
- | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
^ Name ^ ADSP-214xx ^ ADSP-215xx/ | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ | ||
Line 23: | Line 21: | ||
|Gain Envelope| B/S | B/S | S | | |Gain Envelope| B/S | B/S | S | | ||
|Gain Envelope EndlessLoop| B/S | B/S | S | | |Gain Envelope EndlessLoop| B/S | B/S | S | | ||
- | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
Line 30: | Line 27: | ||
|EnvelopeControl| Control | Control Input| | |EnvelopeControl| Control | Control Input| | ||
|Input< | |Input< | ||
- | \\ | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
Line 37: | Line 33: | ||
Note: | Note: | ||
* <fc # | * <fc # | ||
- | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
|------------------------------|----------------------------------------|----------------------------|----------------------------------------------------------| | |------------------------------|----------------------------------------|----------------------------|----------------------------------------------------------| | ||
|Maximum Time|1104 ms|10 to 4400 ms|Time interval in ms| | |Maximum Time|1104 ms|10 to 4400 ms|Time interval in ms| | ||
- | |GainValue_Point< | + | |GainValue_Point< |
- | |Time(ms)_Point< | + | |Time(ms)_Point< |
|NumChannels|2|20|Number of input channels. Change in this value requires re-compilation| | |NumChannels|2|20|Number of input channels. Change in this value requires re-compilation| | ||
|GainEnvelopeType|Generic Gain Envelope|NA |Gain Envelope types. Change in this value requires re-compilation| | |GainEnvelopeType|Generic Gain Envelope|NA |Gain Envelope types. Change in this value requires re-compilation| |