This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:filters:generaleqsingleblend [19 Jan 2021 05:34] Krithika Manchale [DSP Parameters] |
resources:tools-software:sigmastudiov2:modules:filters:generaleqsingleblend [15 May 2021 15:40] Sreesha Y M [DSP Parameters] |
||
---|---|---|---|
Line 32: | Line 32: | ||
General Equalizer module with Single Ext blend factor(General Eq Ext Blend).\\ | General Equalizer module with Single Ext blend factor(General Eq Ext Blend).\\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ADSP-SC5xx(Sample)^ADSP-215xx/ADSP-SC5xx(Block)^ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/SC5xx ^ ADAU145x/146x ^ |
- | |GeneralEqSingleBlend| Yes | Yes|Yes| Yes| | + | | -------------------------------------- | -------------------- | -------------------------------- | ---------------------------- | |
+ | |GeneralEqSingleBlend|B/S|B/S|S| | ||
+ | |GeneralEqSingleBlendExt|B/S|B/S|S| | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Input0|Audio|Input Channel 0| | |Input0|Audio|Input Channel 0| | ||
|Blend0|Control|External Blend pin for SingleEqExtBlend variant| | |Blend0|Control|External Blend pin for SingleEqExtBlend variant| | ||
Line 43: | Line 46: | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Output0|Audio|Output channel 0| | |Output0|Audio|Output channel 0| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | |Frequency|1000|0 to 96000Hz|Cut-off frequency| | + | |----------------------------------------------------------|---------------------------|---------------------------------------------|----------------------------------------------------------| |
- | |Gain|0 dB|-10 to +10 dB|Filter Gain| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_Boost|0 dB| -10 to +10 dB|Set the boost value for a particular filter curve| |
- | |Q|1.41|1 to 15|Q factor of the filter| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_Frequency|1000|0 to 96000Hz|Cut-off frequency| |
- | |NumChannels|1|1 to 20|Increases or decreases the number of input and output channels. Changing this requires re-compilation| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_Gain|0 dB|-15 to +15 dB|Filter Gain| |
- | |NumStages|1|1 to 20|Increases or decreases the number of filter stages. Changing this requires re-compilation| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_Q|1.41|0.1 to 16|Q factor of the filter| |
- | |Blend |0|0 to 1 |Blend factor for the equalizer module| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_Slope|1|0 to 2|Slope controls filter steepness and therefore the transition between the boost/cut and the flat response.| |
- | |SlewRate |0.01|1 to 1|Defines the rate at which input takes the new value| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_FilterType|Parametric filter|Available filter Types|Controls the type of the filter| |
+ | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_EnabledOrBypassed|True|True/False|Enabled/Disabled the algorithm| | ||
+ | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_Phase|False|True/False|Controls the phase of coefficients in 0 degree or 180 degree phase| | ||
+ | |Stage<fc #ff0000>X</fc>_Slew |0|0 to 1|Slew value for individual filter stages| | ||
+ | |Stage<fc #ff0000>X</fc>_Blend |0|0 to 1|Blend value for individual filter stage| | ||
+ | |NumStages|1|1 to 20 | Number of stages of filter. Change in this value requires re-compilation| | ||
+ | |NumChannels|1| 1 to 20|Number of input and output channels. Change in this value requires re-compilation| | ||
\\ | \\ | ||
+ | Here, * <fc #ff0000> X</fc> - Indicates Stage Number | ||
+ | * <fc #ff0000> Y</fc> - Indicates Filter A/Filter B | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/SC5xx/215xx^ | + | ^ Parameter Name ^ Description ^ ADSP-214xx/SC5xx/215xx ^ ADAU145x/146x ^ |
- | |Stage<fc #ff0000>0</fc>_B0|B0 Filter Coefficient|Float| | + | | ------------------------------------ | ---------------------------------------------------------- | ---------------------------------------- | ---------------------------- | |
- | |Stage<fc #ff0000>0</fc>_B1|B1 Filter Coefficient|Float| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_B0|B0 Filter Coefficient|Float|FixPoint8d24| |
- | |Stage<fc #ff0000>0</fc>_B2|B2 Filter Coefficient|Float| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_B1|B1 Filter Coefficient|Float|FixPoint8d24| |
- | |Stage<fc #ff0000>0</fc>_A1|A1 Filter Coefficient|Float| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_B2|B2 Filter Coefficient|Float|FixPoint8d24| |
- | |Stage<fc #ff0000>0</fc>_A2|A2 Filter Coefficient|Float| | + | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_A1|A1 Filter Coefficient|Float|FixPoint8d24| |
+ | |Stage<fc #ff0000>X</fc>_Filter<fc #ff0000>Y</fc>_A2|A2 Filter Coefficient|Float|FixPoint8d24| | ||
+ | |Stage<fc #ff0000>X</fc>_Slew_Lambda|Exponential decay value of filter stage X|Float|FixPoint8d24| | ||
\\ Here, | \\ Here, | ||
- | * <fc #ff0000> Red</fc> - Stage Number (Changes for each stage coefficients) | + | * <fc #ff0000> X</fc> - Stage Number (Changes for each stage coefficients) |
+ | * <fc #ff0000> Y</fc> - Filter A/B for each stage X | ||
\\ | \\ |