This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:rmscompressor [15 Jan 2021 10:56] – [RMS Compressor] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:rmscompressor [12 May 2021 09:36] – John Joseph | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | [[resources/ | + | [[resources/ |
====== RMS Compressor ====== | ====== RMS Compressor ====== | ||
\\ | \\ | ||
Line 7: | Line 7: | ||
===== Description ===== | ===== Description ===== | ||
The RMS Compressor block computes the RMS level of the input signal and applies the compressor gain to the input signal based on the RMS value. | The RMS Compressor block computes the RMS level of the input signal and applies the compressor gain to the input signal based on the RMS value. | ||
+ | \\ | ||
+ | ===== Variants ===== | ||
+ | - RMS Compressor | ||
+ | - RMS Compressor with Gain Out | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name |
- | |RMS Compressor| | + | | -------------------------------------------------------- | ---------------------------- | -------------------------------- | ---------------------------- | |
+ | | RMS Compressor | B/S | B/S | S | | ||
+ | | RMS Compressor with Gain Out | NA | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Input1|Audio|Input channel1| | |Input1|Audio|Input channel1| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Output1|Audio|Output channel1| | |Output1|Audio|Output channel1| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | | ---------------------------------------------- | ||
|TimeConstant|121| 1 to 8686 dB/ | |TimeConstant|121| 1 to 8686 dB/ | ||
|Hold|0 ms|0 to 2000 ms|Controls the time (in ms) the compressor maintains its current output | |Hold|0 ms|0 to 2000 ms|Controls the time (in ms) the compressor maintains its current output | ||
Line 31: | Line 40: | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^Parameter Name^Description^ADSP-214xx/ |
- | |TimeConstant|RMS time constant value|Float| | + | |------------------------------ |------------------------------------------ |-------------------------------------------| ---------------------------------------------- | |
- | |Hold|Hold value|Float| | + | |TimeConstant|RMS time constant value|Float| 8.24 format| |
- | |Decay|Decay value|Float| | + | |Hold|Hold value|Float| 8.24 format| |
- | |Table|Table values | Float| | + | |Decay|Decay value|Float| 8.24 format| |
- | |LogCoeff| Constant coefficients|Float| | + | |Table|Table values | Float| 8.24 format| |
+ | |LogCoeff| Constant coefficients|Float| 8.24 format| | ||
\\ | \\ | ||
===== DSP Parameter Computation ===== | ===== DSP Parameter Computation ===== |