This is an old revision of the document!
Click here to return to the Dynamic Processors page
The RMS Compressor block computes the RMS level of the input signal and applies the compressor gain to the input signal based on the RMS value.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
RMS Compressor | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
Input1 | Audio | Input channel1 |
Name | Type | Description |
---|---|---|
Output1 | Audio | Output channel1 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
TimeConstant | 121 | 1 to 8686 dB/s | Controls the time constant (TC) in dB/second that is used for calculating the RMS input value. The time constant determines how rapidly the compressor will respond to input signal level changes, e.g. the “Attack” time. |
Hold | 0 ms | 0 to 2000 ms | Controls the time (in ms) the compressor maintains its current output gain setting before it starts decreasing as the input level decrease. |
Decay | 10 dB/s | 0 to 10000 dB/s | Controls the rate at which the compressor gain decreases in response to decrease in the input signal level, e.g. the “Release” time. |
SoftKnee | False | True/False | Soft-knee lets the compressor ease into action, making a less-abrupt change from unprocessed signal to compressed signal. If it is not activated, the default is hard-knee behavior, in which compression rate reduces or increases abruptly with the threshold level |
Table | All values are 1 | - | Table values are the gain points used to apply for input signal level |
IsDBps | True | True/False | Enable /Disable the control's Decay and TimeConstant either in dB or linear |
NumChannels | 1 | 1 to 20 | Number of input and/or output channels. Change in this value requires re-compilation |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
TimeConstant | RMS time constant value | Float |
Hold | Hold value | Float |
Decay | Decay value | Float |
Table | Table values | Float |
LogCoeff | Constant coefficients | Float |
TimeConstant = Abs(1 - 10^(TimeConstant/(10 * (FS + 0.0000001)))), Where TimeConstant is 20000/TimeConstant in dBps
Decay = (20000/Decay)/(FS + 0.0000001) (When Decay is in dBps) or Decay/(FS + 0.0000001) (When Decay is in linear)
Hold = FS * Hold/1000
Where FS is the sampling rate