Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:tools-software:sigmastudiov2:modules:basic:pulsecounter [08 Nov 2019 10:28] – created Sanjeeva Reddyresources:tools-software:sigmastudiov2:modules:basic:pulsecounter [14 Sep 2022 13:54] (current) – [Description] Angu Sewa
Line 1: Line 1:
 [[resources/tools-software/sigmastudiov2/modules/basic|Click here to return to the Basic page]] [[resources/tools-software/sigmastudiov2/modules/basic|Click here to return to the Basic page]]
 ====== Pulse Counter ====== ====== Pulse Counter ======
 +{{:resources:tools-software:sigmastudiov2:modules:basic:pulsecounter.png?nolink}}
 ===== Description ===== ===== Description =====
-The Pulse Counter block, counts the number of non inputs received. The pulse counter is to count the number of pulses in specified amount of time. The time is dictated by the signal on StartStop input pin. When the StartStop pin is high, counter starts counting pulses, otherwise the last count value is output. The Reset pin clears the count value and start from zero when StartStop pin is high. +The Pulse Counter block, counts the number of inputs received. There is a start/stop pin to initiate and pause the count, and also a reset pin to set the count back to zero. Any non-zero input on the pulse input pin, is considered a pulse and will be counted when the count is enabled. 
 +\\ 
 +The pulse counter is to count the number of pulses in specified amount of time. The time is dictated by the signal on StartStop input pin. When the StartStop pin is high, counter starts counting pulses, otherwise the last count value is output. The Reset pin clears the count value and start from zero when StartStop pin is high.  
 ===== Targets Supported ===== ===== Targets Supported =====
-^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ADSP-SC5xx(Sample)^ADSP-215xx/ADSP-SC5xx(Block)+^ Name            ^ ADSP-214xx ^ ADSP-215xx/SC5xx ^ ADAU145x/146x ^ 
-|Pulse Counter| Yes Yes|YesYes| +| ------------------------------------------------------------ | -------------------- | -------------------------------- | ---------------------------- | 
 +|Pulse Counter| B/S B/S |
 ===== Pins ===== ===== Pins =====
 ==== Input ==== ==== Input ====
 ^Name^Type^Description^ ^Name^Type^Description^
-|StartStop|Control|Starts/Pause the counter| +|------------------------------|------------------------------------------------------------|------------------------------| 
-|Reset|Control|Resets the counter value| +|StartStop |Control | Starts/Pause the counter| 
-|PulseIn|Control|Input to the counter|+|Reset |Control | Resets the counter value| 
 +|PulseIn | Control | Input to the counter|
 ==== Output ==== ==== Output ====
 ^Name^Type^Description^ ^Name^Type^Description^
-|CountResult|Control|Outputs the count of non zero inputs to the counter| +|------------------------------|------------------------------------------------------------|------------------------------| 
- +|CountResult | Control | Outputs the count of non zero inputs to the counter| 
-===== Configurable Parameters ===== +\\
-No COnfigurable parameters +
-===== DSP Parameters ===== +
-No DSP parameters +
  
resources/tools-software/sigmastudiov2/modules/basic/pulsecounter.1573205336.txt.gz · Last modified: 08 Nov 2019 10:28 by Sanjeeva Reddy