Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:tools-software:sigmastudiov2:modules:basic:fractionaldelay [14 Sep 2022 12:46] – Updates Image and Description Angu Sewa | resources:tools-software:sigmastudiov2:modules:basic:fractionaldelay [14 Sep 2022 12:51] (current) – Updates Description Angu Sewa |
---|
{{:resources:tools-software:sigmastudiov2:modules:basic:fractionaldelay.png}} | {{:resources:tools-software:sigmastudiov2:modules:basic:fractionaldelay.png}} |
===== Description ===== | ===== Description ===== |
The Multi Channel Multi Tap Delay cell provides a variable delay for each output from one of the selected input channel. Each input signal is called as channel and output is called as Tap. The amount of delay for each tap can be modified in real time by updating the current delay. | The Fractional Delay cell provides a variable delay to a single audio input. The input is delayed by the amount reflected in the percentage text box and allows for fractional delays (fractions of a sample period via linear interpolation). The top drop-down menu labeled Max represents the largest amount of delay that could be applied to the input signal and sets the data delay buffer size. |
\\ | \\ |
===== Targets Supported ===== | ===== Targets Supported ===== |