This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:adialgorithms:esc [18 Mar 2021 02:21] – created John Joseph | resources:tools-software:sigmastudiov2:modules:adialgorithms:esc [13 May 2021 06:23] (current) – John Joseph | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== Enhanced Stereo Capture ====== | ====== Enhanced Stereo Capture ====== | ||
+ | |||
+ | {{: | ||
+ | \\ | ||
+ | ===== Description ===== | ||
+ | The Enhanced Stereo Capture (ESC) algorithm takes a stereo record-signal and creates a wider stereo image. The ESC is meant as a record algorithm in order to capture an enhanced stereo image from two closely spaced microphones. | ||
+ | \\ | ||
+ | \\ | ||
+ | ===== Usage ===== | ||
+ | The ESC algorithm accepts two input signals obtained from two closely spaced microphones. The algorithm separates these two signals and widens the stereo image. The end perceptual result is a widened stereo image as if the audio had been captured by microphones with greater L/R separation. The algorithm is based on proprietary filtering and a Stereo Balance Gain that adjusts how much stereo effect is archived in the algorithm. | ||
+ | |||
+ | Depending on the spacing of the microphones in the record environment, | ||
+ | |||
+ | - Simulated delay between the microphones to maximize the L/R separation | ||
+ | - Listening tests while adjusting the gain knob | ||
+ | |||
+ | The tuning required for method 1) can be done within SigmaStudio. The schematic image in example section shows how this is accomplished. The goal is to adjust the Stereo Balance Gain until the greatest visual difference in level is achieved between the left and right output signals.. | ||
+ | \\ | ||
+ | \\ | ||
+ | ===== Targets Supported ===== | ||
+ | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ | ||
+ | | -------------------------------------- | -------------------- | -------------------------------- | ---------------------------- | | ||
+ | | Enhanced Stereo Capture | ||
+ | \\ | ||
+ | ===== Pins ===== | ||
+ | ==== Input ==== | ||
+ | ^ Name ^ Type ^ Description ^ | ||
+ | | ---------------------- | -------------- | ---------------------- | | ||
+ | |LeftIn| Audio | First input channel | | ||
+ | |RightIn| Audio | Second input channel | | ||
+ | |||
+ | ==== Output ==== | ||
+ | ^ Name ^ Type ^ Description ^ | ||
+ | | ---------------------------- | -------------- | ---------------------- | | ||
+ | |LeftOut| Audio | First output channel | | ||
+ | |RightOut| Audio | Second output channel | ||
+ | \\ | ||
+ | ===== Configurable Parameters ===== | ||
+ | ^ GUI Parameter | ||
+ | | ---------------------------------------- | ---------------------- | ------------------ | ---------------------------------------- | | ||
+ | | LRValue | 0dB | -20 - 20dB | This gain knob control adjusts how much stereo effect is achieved in the algorithm. Depending on the spacing of the microphones in the record environment, | ||
+ | \\ | ||
+ | ===== DSP Parameters ===== | ||
+ | ^ Parameter Name ^ Description ^ ADAU145x/ | ||
+ | | ---------------------------------------- | ---------------------------------------------------------------- | ---------------------------------------- | | ||
+ | | gain | Linear gain value | 8.24 Format | | ||
+ | | a1hpf | High pass filter coefficients | 8.24 Format Array | | ||
+ | | a1lpf | Low pass filter coefficients | 8.24 Format Array | | ||
+ | \\ | ||
+ |