This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:adialgorithms:dynamicenhancement [04 Feb 2020 06:00] – Added an image Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:adialgorithms:dynamicenhancement [11 May 2021 07:34] – Formatting updated John Joseph | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |Dynamic Enhancement (Mono)| | + | | ------------------------------------------------ | -------------------- | -------------------------------- | ---------------------------- | |
- | |Dynamic Enhancement (Stereo)| | + | | Dynamic Enhancement (Mono) | B/S |
+ | | Dynamic Enhancement (Stereo) | B/S | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ---------------------- | -------------- | ---------------------- | | ||
|Input0|Audio|Input channel0| | |Input0|Audio|Input channel0| | ||
|Input1|Audio|Input Channel1 (only for stereo)| | |Input1|Audio|Input Channel1 (only for stereo)| | ||
==== Output ==== | ==== Output ==== | ||
+ | ^Name^Type^Description^ | ||
+ | | ---------------------- | -------------- | ---------------------- | | ||
|Output0|Audio|Output channel0| | |Output0|Audio|Output channel0| | ||
|Output1|Audio|Output channel1 (only for stereo)| | |Output1|Audio|Output channel1 (only for stereo)| | ||
Line 30: | Line 34: | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | | ---------------------------------------- | ---------------------- | ------------------ | ---------------------------------------- | | ||
|TimeConstant| 100 ms| 0 to 500ms | This controls the RMS time constant for the detector. Changing the attack and release rates| | |TimeConstant| 100 ms| 0 to 500ms | This controls the RMS time constant for the detector. Changing the attack and release rates| | ||
|CompThreshold| -5 db| -24 to 20 dB|Threshold of the detector.Any signal coming into the detector below the threshold level will not influence the boost calculation. it receives a fixed enhancement.| | |CompThreshold| -5 db| -24 to 20 dB|Threshold of the detector.Any signal coming into the detector below the threshold level will not influence the boost calculation. it receives a fixed enhancement.| | ||
Line 37: | Line 42: | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^ Parameter Name |
+ | | ---------------------------------------- | ------------------------------------------------------------------------------------------ | ---------------------------------------- | | ||
|CompThreshold|Threshold of the detector|Float| | |CompThreshold|Threshold of the detector|Float| | ||
|TimeConstant|Rms time constant for the detector for change in input signal level|Float| | |TimeConstant|Rms time constant for the detector for change in input signal level|Float| | ||
|BoostFrequency|maximum dynamic enhancement gain applied to the algorithm|Float| | |BoostFrequency|maximum dynamic enhancement gain applied to the algorithm|Float| | ||
|BassFrequency|Cut off frequency for the boosting filter|Float| | |BassFrequency|Cut off frequency for the boosting filter|Float| |