This is an old revision of the document!
Return to the parent page
PC Software Setup
ADSP-214xx/ADSP-215xx/ADSP-SC5xx
Install the following software/tools in the listed order:
CrossCore Embedded Studio - SigmaStudio uses the tools that are included with CrossCore Embedded Studio. Install CrossCore Embedded Studio, if it is not already installed on the SigmaStudio+ Host PC.
-
Install SigmaStudio+ version 2.0.0 Eval -
ADI_SigmaStudioPlus-Rel2.0.0_EVAL.exe
Note that if more than one version of the CrossCore Embedded Studio tool-chain is detected, the Processor Settings of
ADSP-214xx/
ADSP-215xx/
ADSP-SC5xx allows for tool-chain selection.
ADAU145x/ADAU146x
Install SigmaStudio+ version 2.0.0 -
ADI_SigmaStudioPlus-Rel2.0.0.exe