Wiki

This version is outdated by a newer approved version.DiffThis version (20 Sep 2022 14:49) was approved by Ashwin PS.The Previously approved version (29 Apr 2022 15:01) is available.Diff

This is an old revision of the document!


Return to the parent page

PC Software Setup

ADSP-214xx/ADSP-215xx/ADSP-SC5xx


Install the following software/tools in the listed order:

  1. CrossCore Embedded Studio - SigmaStudio uses the tools that are included with CrossCore Embedded Studio. Install CrossCore Embedded Studio, if it is not already installed on the SigmaStudio+ Host PC.
  2. Install SigmaStudio+ version 2.0.0 Eval - ADI_SigmaStudioPlus-Rel2.0.0_EVAL.exe
Note that if more than one version of the CrossCore Embedded Studio tool-chain is detected, the Processor Settings of ADSP-214xx/ADSP-215xx/ADSP-SC5xx allows for tool-chain selection.

ADAU145x/ADAU146x

  1. Install SigmaStudio+ version 1.3.0 Eval - ADI_SigmaStudioPlus-Rel1.3.0_EVAL.exe
resources/tools-software/sigmastudiov2/gettingstarted/swsetup.1663678133.txt.gz · Last modified: 20 Sep 2022 14:48 by Ashwin PS