EV-21593-SOM with EV-SOM-CRR EZ-Kit Connections
The board settings for running SigmaStudio+ EV-21593-SOM with EV-SOM-CRR EZ-Kit, using the Default Application is given in the below tables.
Switch | Setting |
---|---|
SW1 | BOOT Mode Switch Default Position 0 |
Switch Settings for EV-21593-SOM Board
Jumper | Setting |
---|---|
JP1 | 2-3 connected |
Jumper Settings for EV-21593-SOM Board
Port | Setting |
---|---|
P1 | Debug port connected to ADZS-ICE-2000/ICE-1000 |
Port Settings for EV-21593-SOM Board
Switch | Setting |
---|---|
SW1 (CRR) | OFF, OFF, OFF, OFF, OFF, OFF |
Switch Settings for EV-SOM-CRR EZ-Kit
Jumper | Setting |
---|---|
JP1 | Not connected |
JP2 | Not connected |
Jumper Settings for EV-SOM-CRR EZ-Kit
Port | Setting |
---|---|
P3 | Connected with SigmaStudio USBi |
P8 | Connected to Power |
J3(SOMCRR) – J2 (SOM) | Connected |
J6(SOMCRR) – J1 (SOM) | Connected |
J5(SOMCRR) – J2 (SOM) | Connected |
Port Settings for EV-SOM-CRR EZ-Kit