Wiki

This version (04 May 2022 14:49) was approved by John Joseph.The Previously approved version (10 Feb 2021 09:46) is available.Diff

Return to the parent page

ADSP-215xx/ADSP-SC5xx Hardware Setup

Requirements

The following are the list of hardware components required for setting up the demo application.

  • ADSP-21569/ADSP-SC573/ADSP-SC584/ADSP-SC589 EZ-Board, EV-21569/21593/SC594 SOM Boards with carrier board and ADSP-SC589 MINI BOARD. ADSP-21573/ADSP-21584 processor mounted on ADSP-SC573/ADSP-SC584 EZ-BOARD.
  • PC/Laptop with a stereo audio out and USB port.
  • ADZS-ICE-2000/ICE-1000 emulator for downloading/debugging/flashing the framework to the Target.
  • EVAL-ADUSB2EBZ USB to SPI converter.
  • Aardvark I2C/SPI Host Adapter
  • Audio cables and USB cables.


Setup

The SigmaStudio+ demonstration setup for ADSP-SC5xx/ADSP-215xx includes a Host PC running SigmaStudio+ which is connected to the ADSP-SC573/ADSP-SC584/ADSP-SC589/ADSP-21584/ADSP-21573/ADSP-21569 EZ-Board. The connection is achieved using a USB-to-SPI converter. The EVAL-ADUSB2EBZ or Aardvark I2C/SPI acts as the USB-to-SPI converter, which is connected to the PC through a USB port and to the Target EZ-Board through SPI lines. The basic steps to set up the Target for SigmaStudio+ demonstration are given below. The setup required to run the demo application is illustrated in below figure.


Connections

Connect EZ-BOARD to PC using USBi

Connect EVAL-ADUSB2EBZ to the PC running SigmaStudio using a USB cable. The EVAL-ADUSB2EBZ (hereafter referred to as the ‘USBi’) has a 10-pin socket. This socket should be connected to the header P2 (marked SIGMASTUDIO) on EZ-BOARD. When connected, Pin 1 of the USBi socket should match pin 1 of header P2 on the EZ-BOARD. This connection is used to download SigmaStudio packets from host PC to the EZ-BOARD.
The USBi to EZ-board connection (direction) is different across different EZ-Boards. Please refer to figures in above links on how to connect to the specific EZ-Board.

Connect EZ-Board to PC using Aardvark I2C/SPI Host Adapter

Connect Aardvark I2C/SPI Host Adapter to the PC running SigmaStudio using a USB cable. Aardvark I2C/SPI Host Adapter has a 10-pin socket. This socket should be connected to the header P2 (marked SIGMASTUDIO) on EZ-BOARD. When connected, Pin 1 of the USBi socket should match pin 1 of header P2 on the EZ-BOARD. This connection is used to download SigmaStudio packets from host PC to the EZ-BOARD.
The Aardvark to EZ-board connection (direction) is different across different EZ-Boards. Please refer to figures in above links on how to connect to the specific EZ-Board

Connect to PC using ICE-2000/ICE-1000

Connect ADZS-ICE-2000/ICE-1000 to the PC running SigmaStudio using a USB cable. In case of ADZS-ICE-2000, the ribbon cable of ICE-2000 should be connected to header P1 (marked DEBUG) on EZ-BOARD. In case of ICE-1000, connect header J2 of ICE-1000 directly to header P1 (marked DEBUG) on EZ-BOARD. This connection is used to download/debug/flash the framework to the target.

Connect Audio Input and Output

Connect an analog audio source and headphones/speakers to the audio ports on the EZ-KIT.

Connect Power to the EZ-KIT

Connect the power and reset the board by pressing the ‘RESET’ button on the EZ-BOARD.

Switch/Jumper/Port Settings

resources/tools-software/sigmastudiov2/gettingstarted/adsp-215xx_and_adsp-sc5xx.txt · Last modified: 29 Apr 2022 15:13 by John Joseph