ADSP-SC589 MINI Board Connections
The board settings for running SigmaStudio on ADSP-SC589 MINI BOARD, using the Default Application is given in the below tables.
Switch | Setting |
---|---|
SW2 | Reset |
SW3 | Not Used |
SW4 | Not Used |
Switch Settings for ADSP-SC589 MINI BOARD
Jumper | Setting |
---|---|
JP1 | Boot Mode (1 and 2 connected for SPI boot) else disconnected |
Jumper Settings for ADSP-SC589 MINI BOARD
Port | Setting |
---|---|
P1 | Debug port connected to ADZS-ICE-2000/ICE-1000 |
P2 | Connected with SigmaStudio USBi |
P3 | Connected to Power |
Port Settings for ADSP-SC589 MINI BOARD