ADSP-SC589 Board Connections with USBi
ADSP-SC589 Board Connections with AARDVARK
The board settings for running SigmaStudio on ADSP-SC589 EZ-BOARD, using the Default Application is given in the below tables.
Switch | Setting |
---|---|
SW1 | Position 0 |
SW5 | ON, OFF, ON, OFF, ON, OFF |
SW6 | ON, OFF, ON, OFF, OFF, OFF |
Switch Settings for ADSP-SC589 EZ-BOARD
Jumper | Setting |
---|---|
JP1 | Connected |
Jumper Settings for ADSP-SC589 EZ-BOARD
Port | Setting |
---|---|
P2 | Connected with SigmaStudio USBi |
P14 | Connected |
P15 | Connected |
P16 | Connected |
P17 | Connected |
P18 | Connected |
P19 | Connected |
P21 | Connected |
P23 | All 3 pairs of jumpers are connected |
Port Settings for ADSP-SC589 EZ-BOARD