The following are the list of hardware components required for setting up the demo application.
The SigmaStudio+ demonstration setup for ADSP-214xx includes a Host PC running SigmaStudio+ which is connected to the ADSP-21489 EZ-KIT Lite. The connection is achieved using a USB-to-SPI converter. The EVAL-ADUSB2EBZ or Aardvark I2C/SPI acts as the USB-to-SPI converter, which is connected to the PC through a USB port and to the Target EZ-KIT Lite through SPI lines using ADZS-USBI2EZB. The basic steps to set up the Target for SigmaStudio+ demonstration are given below.
The EVAL-ADUSB2EBZ (hereafter referred to as the ‘USBi’) has a 10 pin socket and each EZ-KIT has a different header to which the SPI lines connect. Hence an adapter board ADZS-USBI2EZB (hereafter referred to as the ‘adapter board’) is used to connect the USBi socket to the EZ-KIT. The adapter board connects to the primary SPI of the respective EZ-KIT. The USBi should be connected to P1 of the adapter board. When connected, Pin 1 of the USBi socket should match pin 1 of header P1 on the adapter board. LED1 on the adapter board is ON only if the connection is correct.
Connect Aardvark I2C/SPI Host Adapter to the PC running SigmaStudio using a USB cable. Aardvark I2C/SPI Host Adapter has a 10 pin socket and each EZ-KIT has a different header to which the SPI lines connect. Hence an adapter board ADZS-USBI2EZB (hereafter referred to as the ‘adapter board’) is used to connect the Aardvark socket to the EZ-KIT. The adapter board connects to the primary SPI of the respective EZ-KIT. The Aardvark should be connected to P1 of the adapter board. When connected, Pin 1 of the Aardvark socket should match pin 1 of header P1 on the adapter board. LED1 on the adapter board is ON only if the connection is correct.
Connect an analog audio source and headphones/speakers to the audio ports on the EZ-KIT.
Connect the power and reset the board by pressing the ‘RESET’ button on the EZ-BOARD.