This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:output_window [30 Jun 2020 17:17] – created Sreesha Y M | resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:output_window [15 Mar 2024 14:14] (current) – spelling Arpit Arora | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
\\ | \\ | ||
- | |||
====== Output Window ====== | ====== Output Window ====== | ||
- | {{: | + | {{: |
+ | \\ | ||
+ | \\ | ||
+ | All the output log messages, including error messages, generated upon project linking, compiling, and other actions performed on the project are displayed on the Output Window. By default, this window is docked at the bottom of the application. SigmaStudio+ navigates and highlights the source of error when user clicks on any error message displayed on the output window. | ||
+ | \\ | ||
+ | \\ | ||
+ | Following additional features are provided on the Output Window: | ||
+ | - **Clear Entries** - Clears the contents of the output window, which will be enabled only when the output window is not empty. | ||
+ | - **Copy To Clipboard** - Copies the entire output window content to clipboard. | ||
+ | - **Enable Logging** - - Enables logging functionality of the output window. Once enabled, every entry in the output window will be written to the file “OutputWindowLog_< |