This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudiov2:comparison [07 Dec 2022 10:01] – created John Joseph | resources:tools-software:sigmastudiov2:comparison [27 Jan 2023 13:58] (current) – Additional points added John Joseph | ||
---|---|---|---|
Line 4: | Line 4: | ||
====== SigmaStudio | ====== SigmaStudio | ||
\\ | \\ | ||
- | | | + | | |
^ OS, Installer, Supported Targets | ^ OS, Installer, Supported Targets | ||
- | |left | + | |**OS Supported** |
- | | xxxxxxxxxxxx | + | |**Installers** |* ADI_SigmaStudio-Relx.y-x64.exe - SigmaDSP, Codecs and Power Amps support \\ * SigmaStudioForSHARC-SH-Relx.y.z_< |
+ | |**Command line execution (without launching the UI)** |Not supported |Supported | | ||
+ | |**Scripting Interface** |Supported through COM Compliant APIs. Limited application operations and module controls are supported |Supported through Apache Thrift. Wider application operations and modules controls are supported | | ||
+ | |**Supported Targets** |Sigma 100 \\ Sigma 200 \\ Sigma 300/350 \\ SHARC/ | ||
+ | |**Inbuilt Software Update** |Not Supported | Supported | | ||
+ | |**Multi-Application Instance** |Only single instance supported. Multiple projects can be opened simultaneously in the instance | Multiple instances of the application can be launched simultaneously. Only one project per instance at a time. | | ||
+ | |**Version Controllable Projects Files** | ||
^ User Interface | ^ User Interface | ||
- | |left | + | |**Visual Design** |
- | | xxxxxxxxxxxx | + | |**Color Themes** |
- | + | |**Zoom/ | |
- | + | |**Multiple Application Layout** | Not supported| 2 customizable layouts are supported. Switch between these layouts with a single click | | |
- | + | |**Mini-Map for Navigation** |Not supported |Supported | | |
+ | |**Error Highlighting** |Not supported |Supported | | ||
+ | |**Output Console Window** |Not supported |Supported | | ||
+ | ^ | ||
+ | |**Search Functionality** |Not supported |Supported | | ||
+ | |**Support for Module Variants** |Separately listed. Difficult to select or switch \\ {{: | ||
+ | |**Alternate Signal Flow Diagrams** |Not supported |Supported. Unlimited signal flow diagrams can be added and one of the diagrams can be set as active | | ||
+ | |**Algorithm Designer for Module Integration** |Supported |Supported. More intuitive workflow | | ||
+ | |**Downloadable Addins Manager** |Supported |Supported | | ||
+ | ^ | ||
+ | |**Integration of ADI A2B and Audio Processing** |Not supported |Supported | | ||
+ | |**System Design** |Not supported |Supported. Design projects with DSPs, Codecs, Transceivers etc. | | ||
+ | |**Support for Multi-Core, Multi-Instance DSP Processing** |Supported. UI Representation is not intuitive |Supported using hierarchical representation of project elements using project tree | | ||
+ | |**Independent Tuning Tool** |Not supported |Supported | |