Click here to return to the SigmaStudio+ documentation landing page
![]() | ![]() SigmaStudio+ |
|
OS, Installer, Supported Targets | ||
---|---|---|
OS Supported | Only Windows | Only Windows |
Installers | * ADI_SigmaStudio-Relx.y-x64.exe - SigmaDSP, Codecs and Power Amps support * SigmaStudioForSHARC-SH-Relx.y.z_<release category>.exe - SHARC and Griffin support | Single installer ADI_SigmaStudioPlus-Relx.y.z.exe for tool, SigmaDSP, SHARC, Griffin, Codecs and Power Amps support |
Command line execution (without launching the UI) | Not supported | Supported |
Scripting Interface | Supported through COM Compliant APIs. Limited application operations and module controls are supported | Supported through Apache Thrift. Wider application operations and modules controls are supported |
Supported Targets | Sigma 100 Sigma 200 Sigma 300/350 SHARC/Griffin Codecs Power Amps Future processors from ADI will not be supported | Sigma 300/350 SHARC/Griffin Codecs (Planned) Power Amps (Planned) Future processors from ADI will be supported only on SigmaStudio+ |
Inbuilt Software Update | Not Supported | Supported |
Multi-Application Instance | Only single instance supported. Multiple projects can be opened simultaneously in the instance | Multiple instances of the application can be launched simultaneously. Only one project per instance at a time. |
Version Controllable Projects Files | Binary Project File. Not supported | Text Project File. Easy to find difference/modification and version control |
User Interface | ||
Visual Design | Outdated ![]() ![]() | Modern ![]() ![]() |
Color Themes | Not supported | Possible. Currently only one theme (Dark) supported |
Zoom/Resize/Rotate | Not supported | Supported |
Multiple Application Layout | Not supported | 2 customizable layouts are supported. Switch between these layouts with a single click |
Mini-Map for Navigation | Not supported | Supported |
Error Highlighting | Not supported | Supported |
Output Console Window | Not supported | Supported |
Module Library | ||
Search Functionality | Not supported | Supported |
Support for Module Variants | Separately listed. Difficult to select or switch ![]() | Consolidated into a single module. Easy to use ![]() |
Alternate Signal Flow Diagrams | Not supported | Supported. Unlimited signal flow diagrams can be added and one of the diagrams can be set as active |
Algorithm Designer for Module Integration | Supported | Supported. More intuitive workflow |
Downloadable Addins Manager | Supported | Supported |
Advanced Features | ||
Integration of ADI A2B and Audio Processing | Not supported | Supported |
System Design | Not supported | Supported. Design projects with DSPs, Codecs, Transceivers etc. |
Support for Multi-Core, Multi-Instance DSP Processing | Supported. UI Representation is not intuitive | Supported using hierarchical representation of project elements using project tree |
Independent Tuning Tool | Not supported | Supported |