This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:sigmastudio:tutorials:microcontroller [03 Jan 2021 21:46] – fix links Robin Getz | resources:tools-software:sigmastudio:tutorials:microcontroller [10 Feb 2021 14:30] – fix links Robin Getz | ||
---|---|---|---|
Line 65: | Line 65: | ||
==== ADAU1761 ==== | ==== ADAU1761 ==== | ||
- | The ADAU1761 (referred to as Sigma200) has a similar pinout to the ADAU1701, although I2C pullup resistors are already in place on the board. The evaluation board schematic is available [[resources: | + | The ADAU1761 (referred to as Sigma200) has a similar pinout to the ADAU1701, although I2C pullup resistors are already in place on the board. The evaluation board schematic is available [[adi>media/ |
EVAL-ADAU1761Z also allows Pin 4 of the USBi connector to power the DSP. Again, ensure that your system consumes <500mA from a USB port. | EVAL-ADAU1761Z also allows Pin 4 of the USBi connector to power the DSP. Again, ensure that your system consumes <500mA from a USB port. |